Medical USB Platform

Texas Instruments offers a Continua-certified USB hardware-software platform that implements the Personal Healthcare Device Class (PHDC) along with
IEEE 11073.

As personal healthcare devices become more ubiquitous, companies are developing products with connectivity that allow data to be exchanged easily. PHDC (Personal Healthcare Device Class), which is part of the USB standard, is designed for portable medical and wellness devices to be able to send measurements to USB hosts such as personal computers, cell phones, etc. The Continua Health Alliance has released guidelines for interoperability between various types of devices implementing the USB standard. Texas Instruments offers a USB platform for agent devices that has been certified by the Continua Health Alliance after having passed a rigorous testing procedure. Customers can use the software stacks of this platform to reduce development time for devices that will comply with the medical industry standards such as the Continua Health Alliance.

These stacks are available for use on TI's industry-leading, ultra-low-power MSP430™ MCUs.

TI chose to partner with S3 (Silicon & Software Systems Ltd.) because of their extensive experience with the Continua Health Alliance and with developing code-efficient stacks for low-power MCU's such as the MSP430.

Medical USB Stack Solution Diagram - TI.com

Features

  • USB-IF certified
  • Stacks are part of a Continua-certified hardware + software platform
  • Documentation to enable customers to quickly integrate stacks within their own medical solutions
  • Code efficiency: small flash memory footprint
  • Code examples available for several medical devices
  • Capable of running on TI's MSP430 MCUs

Benefits

  • Reduced development time for personal medical devices
  • Allows customers to use their expertise in implementing their applications rather than developing code for lower-layer APIs and stacks
  • Confidence that TI's platform is already Continua-certified

Getting Started with MSP430 Medical USB

video platform video management video solutions video player

Logo - Continua Certified - TI.com

TI in Medical

Learn more about TI's full portfolio for medical applications.

MSP430F663x

The MSP430F663x series with USB 2 are microcontroller configurations with a high performance 12-bit analog-to-digital (A/D) converter, comparator, and two universal serial communication interfaces (USCI).