IoT made easy

By 2020 there will be 50 billion Internet of Things (IoT) devices* – Create yours today!

The SimpleLink™ SensorTag kit allows quick and easy prototyping of IoT devices. It just works – connect your sensor solution to the cloud in minutes. Get started with Bluetooth® low energy, Sub-1 GHz and IEEE 802.15.4 based protocols (e.g. 6LoWPAN, ZigBee®, etc.) now.

* Source: Gartner, 2015

Buy SimpleLink Dual-Band CC1350 SensorTag kit now
Buy SimpleLink Bluetooth Smart CC2650 SensorTag kit now
apps download android apps download app store
IoT made easy By 2020 there will be 50 billion Internet of Things (IoT) devices – Create yours today!


Apps

sensorTag app from ios

Get the Power of SensorTag kit from iOS

With the SensorTag app, you can build your own iOS app in minutes. It allows quick and easy prototyping of simple sensor applications. The Bluetooth® SensorTag kit supports iBeacon™ technology from Apple.

See list of compatible devices
close
sensortag bluetooth low energy

Supported iOS devices

To use the SensorTag, a Bluetooth Smart (4.0 or newer) device is required and the device API must support Bluetooth low energy. Currently the following iOS devices are supported:

  • iPhone 4S and newer
  • iPad (3rd Generation) and newer
  • iPad mini
  • iPod touch (5th Generation) and newer
sensorTag app from android

Get the Power of the SensorTag kit from Android

The new Android SensorTag app gives you control of all sensors, and configures your SensorTag kit before connecting it to the cloud. The Android SensorTag app can be downloaded on Google Play. The full source code for the app is available here.

See list of compatible devices
close
sensortag bluetooth low energy

Supported Android devices

To use the SensorTag, a Bluetooth Smart (4.0 or newer) device is required and the Android API 18 (Android 4.3) must be supported. For the best experience, Android 5.0 is recommended. The SensorTag app is tested on the following Android devices:

Android 5.0 (Lollipop)

  • Google Nexus 5
  • Google Nexus 6
  • Google Nexus 7

Android 4.4 (KitKat)

  • Samsung Galaxy S4
  • HTC One

Features of the Apps

feature - Scan for SensorTags nearby using Bluetooth Smart

Scan for SensorTag nearby using Bluetooth low energy or Bonjour/mDNS for Wi-Fi

The SensorTag app will scan for SensorTag kits nearby and list them for connection. It allows you to identify the SensorTag kits by address and give them custom names

feature - View sensor data through direct connection or local network

View sensor data through direct connection or local network

Once connected to the SensorTag kit, the app displays sensor data and graphs for all sensors on the SensorTag kit

feature - Configure and control the sensors

Configure and control the sensors

Enable and disable the sensor you need for your application and set the desired update interval for each sensor

feature - Connect to the cloud

Connect to the cloud

Once your SensorTag kit is configured, you can connect to the cloud and see your data online. After completing registration, your data can be viewed anywhere using a web browser or mobile app

feature - Upgrade your SensorTag

Upgrade your SensorTag kit

Use this utility to upgrade your SensorTag kit to the latest version

SensorTag Partners

Cloud
IBM

IBM

Connecting the SensorTag to IBM IoT Foundation service is beautifully simple. Get connected using Quickstart or develop your own prototypes using Node-RED.

Learn more about IBM
Cloud
Temboo

Temboo

Code the Internet of Everything with Temboo. Get auto-generated code for your SensorTag that can trigger 2000+ actions for 100+ APIs, databases and code utilities.

Learn more about Temboo
Development tool
EvoThings

EvoThings

Evothings Studio is a mobile IoT app development tool, making it easy and efficient to develop mobile apps for the SensorTag products. Evothings Studio is free to use and open source. Download and read more here:

Learn more about EvoThings Studio
3D print service
Materialise

Materialise

Materialise is a leader in 3D printing. Modify your SensorTag casing to fit your requirements and order 3D prints online.

Learn more about Materialise
Cloud
Vitanet

Vitanet

VitaNet enables IoT manufacturers to deliver simple, safe, cloud-connected devices to their end customers.

Learn more about Vitanet
Cloud
Enmo

Enmo

Enmo's IoT Over Beacon™ technology enables Developers to rapidly prototype their IoT Smartphone Apps.

Learn more about Enmo
(mobile only link)
Cloud
Atomation

Atomation

Atomation's IoT platform can connect any object to the internet with fast integration. The platform includes a mobile SDK that enables developers to easily build apps for the SensorTag kit and gather big data analytics on the cloud.

Learn more about Atomation
Mobile SDK
Atomation

Thingsquare

Thingsquare is a software platform that uses a unique combination of low-power wireless meshing, Bluetooth® beacons, and an ultra-lightweight Internet of Things (IoT) gateway solution to connect sensors, lights, and other products with their users, via their smartphones.

Learn more about Thingsquare