Texas Instruments Transforms Digital Video in the Car and
Home with Four New DaVinci™ Processors, Priced as Low
as $9.95
New DSP-based digital media processors offer improved video
performance with a 50 percent cost reduction over previous
generations
Bangalore, November 20, 2006 – Continuing to expand
the availability of digital video, Texas Instruments Incorporated
(TI) (NYSE: TXN) is now sampling four new digital signal processor
(DSP)-based digital media processors priced as low as $9.95.
These DaVinci™ processors are tuned for specific markets,
including automotive vision, video security and video telephony.
For more information.
“Automotive vision and driver safety assistance, residential
IP netcams and consumer-class videophones are just a few of
the digital video applications that will change how we experience
our car and home,” said Gerard Andrews, DSP Marketing Manager,
TI. “We have created these parts to ensure our customers are
able to capture these exploding markets, while new low price
points will allow the implementation of digital video in a
completely new realm of applications.”
Improved Video Performance, 50 Percent Cost Reduction: The
four new TMS320DM643x processors, the first DSP-only devices
for DaVinci technology, are providing greater processing power
at a lower price point than ever before. Moore’s Law combined
with improvements to the DSP core and the addition of a video
processing subsystem (VPSS), allow the DM643x processors to
offer improved video performance of up to H.264 video encode
at D1 resolution and a 50 percent cost reduction over previous
DSP digital media processors. The TMS320DM6437, TMS320DM6435,
TMS320DM6433 and TMS320DM6431 also have enough headroom for
networking, user interface and other tasks required to run
the complete system on the DSP.
All four processors feature the new TMS320C64x+™ core
and operate at up to 600 MHz. The C64x+™ core provides
20 percent higher throughput at a given speed than the previous
generation. TMS320C64x™ DSP core was the basis of the
highly successful TMS320DM640/1/2/3 digital media processors,
which has been deployed with more than 300 customers and shipped
in excess of five million units. The VPSS integrates a preview
engine, resizer and on-screen display accelerator to provide
up to a 40 percent performance lift.
Right Performance, Peripheral and Cost Options for Target
Video Markets: Three of the new processors (DM6431, DM6435
and DM6437) offer special features that make them suitable
for automotive video applications, such as lane departure
and collision avoidance. They support the CANbus interface,
a network that enables multiple microcontrollers to communicate
with each other and has become a standard in the automotive
industry. They have also achieved AEC-Q1000 automotive quality
standard, which means they have passed a series of specific
stress tests required for automotive implementation.
“By offering processors specifically suited for video applications
and with automotive-specific interfaces incorporated, TI will
help drive the growth of the automotive vision market. The
DM643x devices incorporate features such as CANbus interface
and AEC-Q100 qualification, which will allow us to incorporate
DSP performance into our vision sensors for driver assistance
systems,” said Roger Appelo, Global Strategy Manager, Active
Safety, Sensata Technologies.
The four processors each provide 80 KB L1D, 32 KB L1P cache/SRAM
and 128 KI L2 Cache SRAM memory. They also include a 32-Bit
DDR2 SDRAM memory controller and an asynchronous 8-Bit wide
EMIF. Other peripherals offered by all four processors include
a 10/100 Ethernet media access controller (MAC), two UARTs,
I2C, SPI, GPIO, McASP and three PWMs. Processors in the class
are available in 16 mm and 23 mm square packages and are pin
compatible.
The four DM643x processors take full advantage of the DaVinci
software and development infrastructure by allowing designers
to focus on the application functionality. Developers are able
to implement video, imaging, speech and audio technology through
simple calls to the DaVinci application programming interface
(API) that manages the implementation of specific codec engines
and matching screen resolution. For example, the developer
can use a simple function call without being concerned with
the details of the actual codec implementation. The DM643x
devices can also be programmed using conventional DSP programming
methods with TI’s best-in-class eXpressDSP™ software
and development tools, including Code Composer Studio™ Integrated
Development Environment.
Samples Available to Begin Development Today: Samples
are available today and devices will be in volume production
in 2Q 2007, priced from $9.95 to $22.95 in 10,000 units. A
complete, robust digital video development platform that leverages
the entire DaVinci technology ecosystem, including the codec
engine, eXpressDSP™ Data Visualization Technology and
digital media software for the DM643x devices will be released
in 2Q 2007. For more information about TI’s DaVinci technology
offerings, including digital media software, authorized software
providers and video system development tools, please see www.thedavincieffect.com.
About Texas Instruments
Texas Instruments Incorporated provides innovative DSP and
analog technologies to meet our customers' real world signal
processing requirements. In addition to Semiconductor, the
company includes the Educational & Productivity Solutions business.
TI is headquartered in Dallas, Texas, and has manufacturing,
design or sales operations in more than 25 countries. Texas
Instruments is traded on the New York Stock Exchange under
the symbol TXN. More information is
located on the World Wide Web
Trademarks: DaVinci, TMS320DM64x, TMS320C64x+, eXpressDSP
and Code Composer Studio are trademarks of Texas Instruments.
All other trademarks and registered trademarks are property
of their respective owners.
Additional Customer Comments:
“The cameras in our ground-breaking home and small business
video security system, LükWerks, have successfully used TI’s
TMS320DM64x™ digital media processors. TI’s new offering
of the lower cost, higher performing DM643x processors ensures
that we will be able to continue offering our customers the
highest-quality video security for the most affordable price
on the market,” said Andrew Hartsfield, chief executive officer,
WiLife.
“TI continues to advance the availability of digital video
applications with DaVinci technology. By offering an affordable
digital media processor that can manage the core processing
required by an IP videophone, TI’s technology allows us to
continue to expand our offerings for this growing market,”
said Stuart Griffin, director, Red Embedded Design. |