Texas Instruments delivers thinnest EMI filters with highest ESD performance

6 OCT 2010 | Uncategorized

DALLAS, Oct. 6  /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced six- and four-channel electromagnetic interference (EMI) filters for LCD display applications, the TPD6F202 and TPD4F202. Electrostatic discharge (ESD) ratings exceed the IEC 61000-4-2 specification by at least three times for contact discharge. Both are 67 percent better than the specification for air-gap discharge. This allows the signal to be transmitted through the device while it filters out the higher frequency RF and electromagnetic interferences (RF/EMI) that can appear as lines on a screen, especially LCD displays. The devices' compact size allows designers to optimize previously wasted space under connectors. Targeted applications include LCD display interfaces and anything that needs RF/EMI filtering on data lines, such as portable applications, cell phones, LCD interfaces, and video connections. Download a datasheet or order free samples here: www.ti.com/tpd6f202-pr.  

Key features and benefits of the TPD6F202 and TPD4F202

  • These new 300-um packages are less than half the thickness of a credit card, or 60 percent shorter than the nearest competitor, allowing designers to take advantage of previously wasted space under connectors.
  • Highest ESD protection rating of +/−25kV with less RF/EMI from the signal antenna to the screen delivers a clearer LCD display.
  • Space-saving WCSP with 0.4 mm lead pitch and flow-through pin-mapping facilitates efficient layout in portable applications.

Availability and pricing

The TPD6F202 and TPD4F202 are available now in the space-saving WCSP package with a suggested resale price of $0.21 and $0.17 in quantities of 1,000, respectively.

Learn more about TI's interface portfolio


About Texas Instruments

Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through manufacturing, design and sales operations in more than 30 countries. For more information, go to www.ti.com  

Trademarks

DeviceNet is a trademark of ODVA. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.