Texas Instruments introduces industry's first zero-drift, 36-V op amp

Device improves sensitivity, accuracy and power for ultra-high precision, low- and high-voltage supply applications

15 AUG 2011 | Uncategorized

DALLAS, Aug. 15, 2011 /PRNewswire/ --Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the industry's first zero-drift, 36-V operational amplifier (op amp). Compared to the competition, the dual-channel OPA2188 provides a 4x improvement in offset voltage drift, 60 percent improvement in initial offset voltage and twice the bandwidth at the same power consumption. The OPA2188 can be used in high- and low-voltage supply applications requiring ultra-high precision, such as test and measurement equipment, electronic weigh scales, medical instrumentation and flow meters. For more information and to order samples, visit www.ti.com/opa2188-pr.

"The OPA2188 combines TI's proprietary zero-drift technology with our precision 36-V processes, providing analog designers with a clean and simple way to solve the challenge of taking precision-level measurements in a high-voltage environment," said Steve Anderson, senior vice president of TI's High Performance Analog business. "Our design teams have achieved leading performance levels for ultra-low noise, EMI and RFI input filtering, and low power consumption. These efforts will help our customers achieve higher efficiencies in applications like control and automation, and higher accuracy in portable medical designs."

Key features and benefits

  • Zero drift architecture, 0.03 uV/degree C, reduces the need for future system calibration.
  • Initial offset voltage of 25 uV enables the highest-resolution sensor measurement in its class.
  • Provides 2 MHz of bandwidth while consuming only 475 uA of quiescent current, which will enable portable medical applications to provide even higher levels of accuracy.
  • Low noise of 8.8 nV/rtHz for high system precision.
  • Input common mode range extending from negative rail to within 1.5 V of the positive rail saves additional circuitry and enables 5-V, single-supply operation.

Tools and support

TI offers a variety of tools and support to speed development with the OPA2188, including:


Availability, packaging and pricing

The OPA2188 is available today in a 3-mm x 5-mm MSOP package or 5-mm x 6-mm SOIC package for a suggested retail price of $1.40 for 1,000 units.

Learn more about TI's precision op amp portfolio by visiting the links below:


About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks

TI E2E is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

TXN-P

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all

Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.