TI introduces industry's most accurate current shunt monitor

Complete single-chip solution provides 10 times greater accuracy than competitors

24 AUG 2011 | Uncategorized

DALLAS, Aug. 24, 2011 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NYSE: TXN) today introduced the industry's most accurate current shunt monitor. With a maximum offset voltage of 10-microvolts (uV) and a maximum gain error of 0.1%, the INA226 is 10 times more accurate than leading competitors. The device is a complete 16-bit, single-chip solution, and provides fully programmable measurements for current, voltage and power across a digital I2C interface. The INA226 benefits designers working with servers, telecom equipment, computers, power management devices and testing equipment, where accurate power measurements are crucial. To order samples and learn more, visit: http://www.ti.com/ina226-pr.

Key features and benefits

  • Single-chip digital solution with I2C interface provides current, voltage and power measurements, simplifying board design and layout constraints with no external mux or ADC required.
  • Industry leading accuracy with a maximum offset voltage of 10-uV and maximum gain error of 0.1 percent results in greater precision at low currents and allows for using smaller shunt resistors, reducing I*R loss.
  • Independently programmable conversion times and sample averaging make it easy to customize to the speed requirements of each system, and reduce software and memory requirements.
  • Maximum quiescent current of 420-uA and maximum shutdown current of 2-uA result in efficient operation that consumes 3.5 percent less power than competitors' discrete solutions, even with the INA226's integrated ADC and power mux.
  • 140-dB common mode rejection ratio (CMRR) and 36-V common mode voltage (CMV) ensure there is little to no change in offset voltage throughout the entire range of operation, simplifying error analysis.

Availability and pricing

The INA226 is available now in a 10-pin MSOP package, priced at $1.30 in quantities of 1,000.

Tools and support

An evaluation model is available for the INA226, priced at $75, featuring a USB interface and software for configuring and monitoring the performance of the device. An IBIS model is also available for designers to evaluate the INA226.

TI's current sensing portfolio

The INA226 is a powerful addition to TI's current shunt technology portfolio. TI pioneered Zero-Drift architecture and offers high-accuracy and low-drift current shunt monitors that are small, low-power and highly integrated.  

For more information and technical support questions, visit the links below:


About Texas Instruments

Texas Instruments semiconductor innovations help 80,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun.  Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities.  This is just the beginning of our story.  Learn more at www.ti.com.

Trademarks

TI E2E is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

 

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.