TI stereo spatial array IC brings immersive audio experience to smartphones and tablets

Configurable spatial processor creates mobile cinematic experience

17 APR 2012 | Uncategorized

DALLAS, April 17, 2012 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced an integrated circuit (IC) that converts a smartphone or tablet computer's narrow soundstage into a much wider and exciting audio experience for consumers. The stereo spatial array IC and companion software tool enable mobile device designers to overcome the limited soundstage of closely spaced speakers by manipulating sounds in 3D space to create a bigger, more immersive cinematic experience. The LM48903 stereo Class D spatial array joins a family of innovative spatial audio ICs designed for space-constrained applications from smartphones to ultra-slim flatscreen TVs. For more information and to order samples, visit www.ti.com/spatial2-pr.

(Photo: http://photos.prnewswire.com/prnh/20120417/DA87541)

Key features and benefits

  • Complete audio solution: IC integrates a spatial processing DSP, two Class D amplifiers, 18-bit stereo analog-to-digital converter (ADC), phase-locked loop (PLL), and I2S and I2C interfaces.
  • Simplified audio effect programming: Easy-to-use software tool speeds development by eliminating the customer's need for algorithm tuning and in-house DSP experts.
  • Immersive audio effect: Enables differentiated products that defy physical system size to provide an expanded soundstage superior to competitive solutions.
  • Integrated 2-W speaker drivers: Two Class D speaker drivers deliver 2 W per channel of continuous output power into a 4-Ohm load with less than 1-percent total harmonic distortion plus noise (THD+N) to simplify system design and reduce bill of materials.

 

Tools and support
The LM48903's web-based Speaker Array Designer tool includes an easy-to-use coefficient generator that creates unique spatial audio coefficients in a few easy steps. Also included are Android drivers and an evaluation board with graphical user interface.

Availability, packaging and pricing
The LM48903 is available today in a 30-bump, 2.7-mm x 3.2-mm micro SMD package. Suggested retail pricing is $1.75 in 1,000-unit quantities.

Learn more about TI's audio portfolio by visiting the links below:

 

About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks
TI E2E is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.