TI introduces industry's first LED controller with constant power regulation
Phase-dimmable LED driver provides smooth, flicker-free dimming
LAS VEGAS, May 9, 2012 /PRNewswire/ -- LIGHTFAIR INTERNATIONAL -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced a new LED controller with constant power regulation. The LM3447 AC/DC LED driver includes a dimmer detect, phase decoder and adjustable hold current circuits to provide smooth and flicker-free dimming operation in off-line, isolated LED lighting applications, including A19, E26/27 and PAR30/38 bulbs, as well as can light retrofits. For more information, samples and an evaluation module, visit www.ti.com/lm3447-pr.
(Logo: http://photos.prnewswire.com/prnh/20010105/NEF016LOGO)
Traditional drivers use constant current control to accurately regulate LED forward current. This approach produces consistent light output or intensity from LEDs in the same bin. However, once current is applied to the LED, its solder point temperature rises, leading to a decrease in forward voltage and a drop in efficacy. Conversely, by using the new LM3447 with constant power regulation, the LED forward voltage droop over temperature is offset by an increase in LED current to maintain constant LED power. The result is up to 10-percent improvement in efficacy across the expected operating temperature range of the fixture. Watch a video at www.ti.com/lm3447v-pr.
The LM3447 joins TI's portfolio of off-line LED lighting controllers that include the National LM3445, the industry's first phase-dimmable LED driver with constant current control, and the TPS92310 primary side regulator for non-dimming applications. For more information on all of TI's lighting products, visit http://www.ti.com/lighting-pr. The LM3447 will be demonstrated in TI's booth #6935 at Lightfair International in Las Vegas, NV, from May 9 to 11.
Key features and benefits of the LM3447 LED driver
- Integrated phase dimmer decoding and dimmer detection circuitry allows for easy design and highest efficiency.
- Operates with leading edge (TRIAC) and trailing edge dimmers.
- Primary side control supports isolated lighting designs without opto-couplers.
- Constant power LED load regulation improves efficacy of LED array by compensating for LED junction temperature changes.
- Fixed frequency discontinuous conduction mode flyback topology with valley switching simplifies EMI filter design.
- Greater than 0.9 power factor correction meets all regulatory requirements.
- Thermal fold-back protects LED array from over-temperature while still providing reduced light output.
- LED open- and short-circuit protection and driver IC thermal shutdown protect lamp electronics from damage during fault conditions.
Availability, packaging and pricing
The LM3447 is available in volume now from TI and its authorized distributors. Offered in a 14-pin TSSOP package, the suggested retail price is $1.15 in 1,000-unit quantities.
Find out more about TI's LED lighting portfolio:
- Order samples and an evaluation module of the new LED driver: http://www.ti.com/lm3447-pr.
- Get more information on all of TI's LED drivers: www.ti.com/lighting-pr.
- Ask questions and share knowledge in the LED forum in the TI E2E™ Community: www.ti.com/ledforum-pr.
- Download LED reference designs from TI's PowerLab™ Reference Design Library: www.ti.com/powerlab-pr.
- Use TI's AC/DC LED driver online navigation tool to create a complete LED drive solution: http://www.ti.com/ww/en/lighting/bulb/selectortool.shtml.
About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
TI E2E and PowerLab are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
SOURCE Texas Instruments Incorporated