TI speeds data rates in highly-loaded CAN networks with new transceivers

Turbo CAN transceivers enhance system timing margins in industrial applications

23 MAY 2012 | Uncategorized

DALLAS, May 23, 2012 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced a family of turbo CAN transceivers designed for data rates in excess of 1 Mbps, meeting the growing demand for more nodes and greater data transmission length in today's industrial CAN networks. The SN65HVD255 and SN65HVD256 devices offer short propagation delay and fast loop times to support higher data rates and deliver more timing margin in these systems. These devices continue TI's CAN innovation and provide a next-generation design path from the SN65HVD251 and SN65HVD1050 transceivers.

The SN65HVD255 and SN65HVD256 provide enhanced protection features compared to the competition, such as transmit data dominant time-out functionality, under voltage lock-out, and robust electrostatic discharge (ESD) protection at +/-12 kV human body model (HBM), to enable reliable system performance. These enhancements optimize industrial applications, such as factory and building automation, process control equipment, and motor control. To download data sheets or order samples see: www.ti.com/turbocan-pr.

Key features and benefits

  • Standards compliance: The new CAN transceivers meet the ISO1189-2 High Speed CAN Physical Layer standard, ensuring interoperability and easing design.
  • Wide data rate range: 1-Mbps operation in highly-loaded CAN networks down to 10 kbps, while including transmit data dominant time-out protection, to support a robust CAN network.
  • "Ideal passive" behavior: When the device is not powered, it appears as high impedance, thereby not loading the system.
  • Extended temperature range: -40 to +125C temperature range supports all industrial applications.

Tools and support

Availability and pricing

The SN65HVD255 and SN65HVD256 are available today in an 8-pin SOIC package. Suggested retail pricing is $0.50 in 1,000-unit quantities. The SN65HVD255DEVM is available for $49.00 each.

Learn more about TI's interface portfolio:

About Texas Instruments

Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks

TI E2E is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.