TI's new DSP software and development kit jump-start real-time signal processing innovation for biometric analytics applications
Scalable development platform features embedded analytics for applications that require fingerprint recognition and face detection
DALLAS, May 24, 2012 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced the TMS320C6748 DSP development kit for real-time analytics applications such as fingerprint recognition and face detection, enabling systems to sense and analyze biometric information for enhanced access control. The C6748 DSP development kit is also ideal for other digital signal processing applications, such as audio and communications. In addition, the C6748 DSP development kit comes pre-loaded with TI's new C6748 SYS/BIOS Software Development Kit (SDK). This scalable development kit, available for the low price of $195, enables fast and easy development on the C6748 floating- and fixed-point DSP.
Easy to write and optimize DSP code
TI's new C6748 SYS/BIOS SDK includes several demonstrations for biometric analytics applications, such as fingerprint recognition and face detection, offering a starting point for developing and demonstrating the real-time intelligence of TI's C674x DSPs. The SDK also includes the latest SYS/BIOS real-time kernel; the C6748 StarterWare software package, which provides lightweight, operating-system-independent software libraries and utilities; Code Generation Tools; as well as DSP core performance benchmarks that show the real-time processing power of TI's C674x DSPs. The C6748 SYS/BIOS SDK enables developers to run demos in less than 10 minutes and begin creating DSP applications in less than one hour. In addition to the SDK, the C6748 DSP development kit includes Code Composer Studio™ integrated development environment (IDE) v5.1
Simple hardware development and expansion
TI's C6748 DSP development kit also speeds and eases hardware development of real-time DSP applications. The board reduces design work with freely downloadable and duplicable board schematics and design files. With a wide variety of standard interfaces for connectivity and storage, developers can easily bring audio, video and other signals onto the board. In addition, expansion headers allow developers to add display and user interface technology, such as the camera board from Leopard Imaging and LCD screens, extending functionality of the development kit.
Software compatibility enables easy portfolio expansion
TI's scalable platform provides a variety of performance, power, peripheral and price options, which gives developers the opportunity to use the platform to create a varied product portfolio of their own. TI's C6748 DSP development kit is software and pin-to-pin compatible across TI's C6748, C6746 and C6742 DSPs and software compatible with other TMS320C6000™ DSPs. In addition, developers can scale to the software and pin-for-pin compatible OMAP-L138 and OMAP-L132 DSP + ARM9™ processors to add high-level operating systems such as Linux as well as control and networking functionality for applications such as industrial control, medical diagnostics, and communications.
Pricing and availability
TI's C6748 DSP development kit is currently available for the low cost of $195. The C6748 SYS/BIOS SDK is pre-loaded with the C6748 StarterWare software package. Developers can obtain the SDK with a single download at TI.com, or download the StarterWare software package separately. The floating- and fixed-point C674x DSP generation is available today for a new low starting price of less than $5 in quantities of 10,000 units.
Additionally, an OMAP-L138 DSP + ARM9 development kit is available today for $195. This kit is supported by a new Linux SDK, which includes the OMAP-L138 StarterWare software package, as well as the GCC 4.5 tool chain, all available at no cost. The SDK enables developers to begin writing code in less than one hour.
Code Composer Studio IDE v5.1 is pre-loaded on both kits or can be licensed starting at $495.
TI also offers the OMAP-L138/C6748 evaluation module (EVM) for full-featured development. The EVM is available for $1,050.
Get smart with TI
TI's embedded analytics technology unites the power of embedded systems with the intelligence of the human senses to enable systems to analyze information and make intelligent decisions. TI offers a robust portfolio of real-time embedded processing system solutions integrated with smart embedded analytics. With these solutions, TI's customers are developing automotive vision, video security, biometric analytics and intelligent industrial applications that make the world smarter, safer and more fun.
For more information
- Check out TI's Power Solutions for TI's C6748 DSP
- Join the TI E2E™ community
- Follow TI on Twitter
- Like TI on Facebook
About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
Code Composer Studio, TMS320C6000 and TI E2E are trademarks of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.
Embedded processor | Digital signal processor | DSP | DSP ARM | ARM9
SOURCE Texas Instruments Incorporated