TI unveils adapter power controller with lowest standby power

Flyback power supply controller with 700-V start-up switch achieves <10 mW of no-load power, meets EU 5-Star rating for low-power AC adapter chargers

12 NOV 2012 | Uncategorized

DALLAS, Nov. 12, 2012 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ:TXN) today introduced a power management controller with a 700-V start-up switch that achieves less than 10 mW of "no-load" standby power in 5- and 10-watt cube adapters used with smartphones and tablets. In addition to the lower power capability, the new UCC28710 primary-side, regulated flyback controller helps designers create smaller cube adapters and AC-powered equipment. For more information and samples, visit: www.ti.com/ucc28710-pr.

The innovative controller maintains an industry-best 78-percent average power efficiency at 5 watts, which allows adapters to meet the European Commission's 5-Star no-load power consumption rating of <30 mW. The UCC28710 also leverages TI's new .25um, 700-V analog process technology, called LBC7HV, to integrate the start-up switch -- saving an additional 8 mW to 10 mW of standby power.

Key features and benefits of the UCC28710:

  • Lowest standby power: achieves <10-mW standby power consumption and provides high-voltage start-up capability.
  • Highest integration with primary-side regulation: eliminates the need for an optocoupler and TL431 feedback circuit; supports widest input voltage range with VDD, resulting in smaller bias capacitors; supports smaller transformers because of its high-frequency operation; and reduces overall design size and complexity without the need for additional external circuits.

Speed time-to-market with adapter charging reference designs
The family of UCC287xx controllers includes the UCC28700, UCC28701 and other products to help customers simplify and speed their adapter designs. A new UCC28710 controller-based 10-W AC Eco-charger for tablets and smartphones design adds to TI's growing PowerLab™ reference design library for AC adapters, universal USB charging cubes and car chargers.

Availability and pricing
The UCC28710 flyback controller is available in a 7-pin, SOIC package and is priced at US$0.42 in quantities of 1,000. The 5-W UCC28711EVM evaluation module is available for ordering through TI's eStore. The module converts a 90-V to 265-V RMS input voltage down to 5 V DC, with a 1-A current limit for USB adapter applications.

Find out more about TI's adapter and charging portfolio:

About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

Trademarks
TI E2E and PowerLab are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.