Industry's first power circuits with MIPI® RFFE maximize battery life in 2G, 3G, 4G LTE smartphones and tablets

TI's new RF power management converters help power amplifiers consume half the power in 50-percent less board space

26 AUG 2013 | Uncategorized

DALLAS, Aug. 26, 2013 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ:TXN) today introduced the industry's first RF power converters to integrate the MIPI Alliance's radio frequency front-end (RFFE) digital control interface, a specification that simplifies multi-band and multi-radio communications. The highly efficient LM3263 buck converter and LM3279 buck-boost converter significantly reduce the heat and power consumption in RF power amplifiers, improving battery life and extending talk time in 2G, 3G and 4G LTE smartphones, tablets and data cards. View an Engineer It video, which outlines how to meet power requirements for the RFFE interface. Order samples at: www.ti.com/lm3263-pr.  

The LM3263 2.5-A buck converter's  average power tracking feature helps it meet stringent RF requirements of multi-mode, multi-band power amplifiers with fast output voltage transients. The device also includes active current assist and bypass to minimize inductor size without loss of output regulation -- resulting in a 10-mm2 solution, which is half the size of competing solutions. The LM3279 1-A buck-boost regulator supports fast output voltage transients for 3G and 4G LTE. The device enables the amplifier to support high output power and high data rates, even at low battery voltages.

Key features and benefits of LM3263 and LM3279:

  • MIPI RFFE digital control interface provides compatibility with next-generation RF front end chipsets, power amplifiers and reference platforms. The 2.5-A LM3263 meets voltage and current requirements of 2G, 3G and 4G, and the LM3279 supports 1-A loads for 3G and 4G.
  • Smallest solution size: The 2.7-MHz LM3263 buck converter results in a 10-mm2 total solution size; and the LM3279 is a 13-mm2 solution.
  • Extends battery run-time: 95-percent efficiency; reduces heat dissipation and cuts battery current consumption through average power tracking with dynamically adjustable output voltage.
  • High performance, low noise: Designed to meet RF and 3GPP requirements, the LM3279 buck-boost supports high linearity and high output power, even at low battery voltages.

TI also introduced the LM8335 general output expander with MIPI RFFE host interface to complement the LM3263 and LM3279. The expander reduces the general-purpose input/output pin allocation and gives designers greater design flexibility to support up to eight additional analog outputs that use analog-controlled, non-MIPI RFFE compliant components.

Easy-to-use evaluation modules

Designers can test power and performance with the LM3263, LM3279 and LM8335 evaluation modules for 3G and 4G RF power amplifiers. The modules include all essential active and passive components to compare analog and RFFE digital control modes of operation.

TI analog for consumer electronics

TI's broad range of power management and analog signal chain products offers design engineers the high performance, low power and integration they need to create innovative and differentiated consumer electronics. TI is engineering the future with gesture recognition, touch feedback, advanced battery charging, audio, health technology and more. Learn how TI analog products improve how we live, work and play at www.ti.com/analogconsumer-pr.

Availability and pricing

The LM3263 comes in a 2-mm x 2-mm x 0.6-mm, 16-bump lead-free DSBGA package, and is priced at US$0.48 in 1,000-unit quantities. The LM3279 buck-boost converter also comes in a 2-mm x 2.5-mm x 0.6-mm, 16-bump lead-free DSBGA package, and is priced at US$0.75 in 1,000-unit quantities.  The LM8335 comes in a 2-mm by 2-mm by 0.6-mm, 16-bump lead-free DSBGA package, and is priced at US$0.68 in 1,000-unit quantities.

Find out more about TI's power portfolio by visiting the below links:

  • TI provides the industry's most comprehensive line of DC/DC adaptive power supply circuits for RF power amplifiers. Search TI's expanding line of RF power management ICs.
  • Ask questions, help solve problems in the Power Forum in the TI E2E™ Community.

About Texas Instruments

Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks

TI E2E is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.