Ultra-low power circuits to enable next wave of energy harvesting design
New TI power harvesters and step-down converters extract and manage the lowest amount of power available from light, thermal and vibration sources
DALLAS, Nov. 18, 2013 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced five new next-generation power management integrated circuits that efficiently acquire and manage microwatts (uW) to milliwatts (mW) of power harvested from light, heat or mechanical energy sources. The bq25570, bq25505, TPS62740, TPS62737 and TPS62736 maintain the industry's lowest levels of active quiescent current and enable battery-free operation to wireless sensor networks, monitoring systems, wearable medical devices, mobile accessories and other applications with limited access to power. To order samples and development kits, visit: www.ti.com/energyharvesting-pr.
To view the multimedia assets associated with this release, please click: http://www.multivu.com/mnr/54051-texas-instruments-next-wave-of-energy-harvesting-design
(Photo: http://photos.prnewswire.com/prnh/20131118/MM16985)
Nano-power harvesting
TI's new bq25570 boost charger with integrated buck converter consumes a miniscule 488 nanoamps (nA) of quiescent current and achieves greater than 90-percent efficiency at output currents lower than 10 microamps (uA), maintaining high efficiency even at the lowest amount of available power. The device features maximum power point tracking (MPPT) to extract and manage power from photovoltaic cells and thermoelectric generators, and supports any energy storage element, such as a rechargeable Li-Ion battery, thin film battery, super-capacitor or conventional capacitor. During long periods of storage, power to the bq25570 can be disabled through a "ship mode" feature, which allows the device to consume less than 5 nA.
The bq25505 boost charger is similar to the bq25570, but achieves an even lower active quiescent current of 325 nA. The bq25505 features a unique, autonomous power multiplexor gate drive that enables seamless system operation from energy harvesting sources and the primary battery, ensuring constant power is available when the system needs to operate, even when no energy is available from the harvester.
Ultra-low power DC/DC converters
In addition to the battery management circuits, TI introduced the TPS62740, the smallest and lowest power buck converter for 300-mA output current designs, providing 360 nA of quiescent current during active operation and 70 nA during standby. The converter achieves greater than 90-percent efficiency down to 10 uA. Achieving a total solution size of 31 mm2, the converter uses a programmable output voltage feature and DCS-Control™ functionality to power microcontrollers, such as TI's ultra-low power MSP430FR59xx microcontrollers (MCUs) and Bluetooth
® low energy solutions, such as the SimpleLink™ CC2541 wireless MCU. The TPS62740's integrated load switch also conserves the power of components like LEDs or sensors that are used temporarily.
For lower current designs, TI's new TPS62737 converter for 200-mA designs and TPS62736 for 50-mA designs provide an ultra-low 370 nA quiescent current during active operation and 15 nA during sleep, while achieving 90 percent efficiency at output currents lower than 15 uA.
Enabling energy harvesting design
As the leading provider of power management integrated circuits and MCUs, TI is taking low-power design to the next level with innovative products that extract and manage energy from ambient sources with the highest efficiency and lowest power consumption. In 2011, TI introduced its bq25504 boost charger circuit with a low quiescent current of 330 nA. TI also provides boost converters, buck converters and battery chargers that support any low-voltage, low-power design requirement.
Availability and pricing
All products are shipping in volume production and are available through TI's worldwide distributor network. The bq25570 and bq25505 come in a 3.5-mm by 3.5-mm QFN package, and are priced at US$3.20 and $2.40, respectively, in 1,000-unit quantities. The TPS62740 comes in a tiny 2-mm by 3-mm SON package, and is priced at US$1.10 in 1,000-unit quantities. The TPS62737 and TPS62736 are available in a 3.5-mm by 3.5-mm QFN package, and are priced at US$1.00 and $0.80, respectively, in 1,000-unit quantities.
Find out more about TI's nanopower power management portfolio by visiting the below links:
- Order evaluation modules for bq25570EVM-206 and bq25505EVM-218 and download the PSpice transient model simulation software for bq25570 and bq25505 to simplify design and reduce development time.
- Evaluation modules for the low-power DC/DC converters include: TPS62740EVM-186, TPS62737EVM-560 and TPS62736EVM-205.
- Search for solutions, get help and share knowledge in the Power Management Forum in the TI E2E™ Community.
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
TI E2E, DCS-Control and SimpleLink are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
SOURCE Texas Instruments