Industry's fastest 16-bit DAC sprints to 2.5 GSPS, supports 12.5 Gbps JESD204B

TI's digital-to-analog converter provides up to 2 GHz of information bandwidth

23 JAN 2014 | Uncategorized

DALLAS, Jan. 23, 2014 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today unveiled the industry's fastest 16-bit digital-to-analog converter (DAC). The 4-channel, 2.5-GSPS DAC38J84 is 66 percent faster than the competition and supports the JEDEC JESD204B serial interface standard for data converters up to 12.5 Gbps. The pin-compatible 2-channel, 16-bit DAC38J82 also runs at 2.5 GSPS, 25 percent faster than existing 16-bit dual DACs. For more information about the DACs and to learn more about TI's growing JESD204B portfolio, visit www.ti.com/dac38j84-pr.

(Photo:  http://photos.prnewswire.com/prnh/20140123/DA50885)

The DAC38J84 and DAC38J82 provide the bandwidth, performance, small footprint and low power consumption needed for multi-mode 2G/3G/4G cellular base stations to migrate to more advanced technologies, such as LTE-Advanced and carrier aggregation on multiple antennas. The DACs support up to 2 GHz of information bandwidth for wideband power amplifier digital pre-distortion, millimeter wave backhaul infrastructure, signal jamming, radar and test equipment.

An interoperability report is available demonstrating the DAC38J84 with Altera's Stratix V and Arria V FPGAs. The report provides the guidance designers need to quickly implement a working link between the FPGA and high-speed DAC.

Key benefits:

  • Widest frequency bandwidths: The DACs provide an input rate up to 1.23 GSPS per DAC. The DAC38J84 provides two independent transmit paths with up to 1 GHz of complex information bandwidth each – 67 percent more than the next fastest quad-channel DAC.
  • Unique multi-band summation: The DAC38J84 is the first quad DAC to integrate a multi-band summation block that allows two complex carrier blocks to be independently mixed to the desired frequency before being summed together for a single path complex transmit. This supports up to 2 GHz of information bandwidth from one pair of 2.5-GSPS output DACs. 
  • Low power: The DAC37J84 consumes only 1100 mW at the common wireless base station condition of 1.474 GSPS, 50 percent lower than existing 4-channel DACs. At 2.458 GSPS, the DAC38J84 uses only 1612 mW.
  • Pin-compatible 1.6-GSPS options: The pin-compatible 4-channel DAC37J84 and 2-channel DAC37J82 run up to 1.6 GSPS.

Tools and support to speed design
Evaluation modules (EVMs) are available to quickly evaluate the performance of the DACs. The DAC38J84EVM, DAC37J84EVM, DAC38J82EVM and DAC37J82EVM include the LMK04828, the industry's first JESD204B clock jitter cleaner, which provides the 2.5-GHz DAC clock and multiple SYSREF signals for full JEDEC JESD204B multi-chip synchronization. An IBIS model is also available to verify board signal integrity requirements.

In 2Q 2014, reference designs will be available for all four DACs. The designs will include the LMK04828 JESD204B clock jitter cleaner and two wideband complex modulator options for a complete bits-to-RF solution up to 4 GHz. Modulator options will include the TRF3705 and an upcoming version of the TRF3705 with integrated PLL/VCO.

Customers can pair any of the DAC EVMs above with the TSW14J56EVM pattern generator and data capture card, and a suitable analog-to-digital converter (ADC) EVM, such as the ADS42JB69EVM, to create a complete transmit and receive evaluation system.

Support is available on the High Speed Data Converters Forum in the TI E2ETM Community, where engineers can search for solutions, get help, share knowledge and solve problems with fellow engineers and TI experts.

Package, availability and pricing
Samples of all four DACs are available today in a 10-mm by 10-mm BGA package. Production quantities are expected in the first half of 2014.

Suggested retail pricing for 1,000-unit quantities is as follows: US$120 for the DAC38J84, US$79 for the DAC37J84, US$70 for the DAC38J82 and US$39.95 for the DAC37J82.

Learn more about TI's data converter portfolio by visiting the links below:

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
TI E2E is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.