First 7-channel, NMOS low-side driver replaces Darlington transistor arrays in high-voltage systems

Drop-in compatible relay driver reduces power, cost and board space

25 JUN 2014 | Uncategorized

DALLAS, June 25, 2014 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced the industry's first seven-channel, NMOS low-side driver, replacing standard Darlington transistor arrays with a power-efficient, drop-in compatible integrated circuit (IC). The TPL7407L replaces half of the transistor arrays required to drive high current loads, providing a new option for high voltage systems that previously required a number of transistor arrays or a motor driver. Reducing power by 40 percent, this new device efficiently drives the LED matrix, relay or stepper motor in high-voltage applications, such as white goods, building automation, lighting and HVAC. For more information or to order samples and an evaluation module, visit www.ti.com/tpl7407l-pr.  

Industry's first 7-channel NMOS low-side driver for high-voltage systems

The TPL7407L complements TI's broad portfolio of peripheral drivers, covering a wide voltage and current range, giving designers the ability to choose a device to suit their needs without extensive system redesign. When used with the SN74HC595 register, one or multiple TPL7404 can be controlled with just three GPIO pins, providing a flexible, efficient solution.

Key features and benefits of the TPL7407L:

  • Highest drain current: With 600 mA per channel, the TPL7407L offers 20 percent better drain current to drive higher power, reducing the number of relay drivers required per board.
  • Highest power efficiency: Supports energy-efficiency in high-voltage systems, reducing power dissipation by 40 percent compared to Darlington arrays.
  • Pin-to-pin compatible with traditional arrays: Replacing existing arrays with this power-efficient device eases system design and frees power budget.
  • Full temperature range: Tested and compatible with the full -40C to 125C temperature range for harsh environments within industrial, automotive and telecommunications applications.

Availability, packaging and pricing
The TPL7407L is available in 16-pin SOIC and TSSOP packages. Suggested retail pricing in 1,000-unit quantities starts at US$0.40. The TPL7407LEVM is also available for US$49.00, providing an easy way to evaluate device performance and operating characteristics.

Learn more about TI's relay driver portfolio :

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors.  By employing the world's brightest minds, TI creates innovations that shape the future of technology.  TI is helping more than 100,000 customers transform the future, today.  Learn more at www.ti.com.

Trademarks
TI E2E is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

Photo - http://photos.prnewswire.com/prnh/20140625/121468

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.