TI drives innovative fusion between infotainment and informational advanced driver assistance systems
New informational ADAS software development kit delivers increased functionality and integration capability without compromising system performance
DETROIT, June 4, 2015 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today announced the availability of its new informational advanced driver assistance systems (InfoADAS) software development kit (SDK). The new SDK delivers an automotive-ready InfoADAS framework for integrating ADAS algorithms into existing in-vehicle infotainment (IVI) systems. A growing industry trend, InfoADAS adds non-active safety information content such as surround view, pedestrian and lane detection and more to traditional IVI features to enhance the driving experience. TI's InfoADAS SDK enables developers to:
- Extend investments in infotainment with the addition of innovative InfoADAS use-cases to enhance the driver's awareness of the conditions inside and outside the vehicle, without compromising the performance of either IVI or InfoADAS systems.
- Reshape traditional infotainment architectures by integrating additional functions on TI's DRA7xx "Jacinto 6" infotainment processors.
To learn more, watch this video about InfoADAS.
Differentiation to support modern automotive cockpit mega-trends
With the increasing deployment of cameras and sensors in vehicles to make the driving experience safer, there is a need to collect, analyze and display further information to the driver without significantly increasing overall R&D investments or bill-of-materials (BOM). The InfoADAS SDK provides scalability across high-level operating systems (HLOS) and "Jacinto 6" devices for reuse of existing designs and resources. It can also be used as a pluggable InfoADAS subsystem to existing head unit applications. To act as a reference for customer's productized algorithm development, the InfoADAS SDK includes sample vision algorithms to demonstrate the framework capabilities, and also includes hooks to extend the framework for higher-level application features (such as park guide overlays). In addition to the existing HLOS SDK supported on the "Jacinto 6" platform and Vision SDK dedicated to control safety functions supported on the TI TDAx processors, the delivery of the InfoADAS SDK unifies the software architecture across TI's automotive processors, "Jacinto" and TDAx, for easy integration and scalability.
TI's "Jacinto 6" family of processors
The DRA7xx family of processors provides a hardware- and software-compatible platform capable to augment existing infotainment products with informational ADAS features. To enable InfoADAS, there is no hardware change required besides upgrading the system to route cameras to the processor. This allows customers to leverage cameras both inside and outside the vehicle together with existing infotainment platforms. Up to four dedicated accelerators, including TI's C66x Digital Signal Processor (DSP) and Embedded Vision Engine (EVE), and other "Jacinto 6" family capabilities allow for concurrencies of head-unit features and emerging analytics and image manipulation not previously possible on a single device.
Pricing and availability
The DRA7xx processors, intended for high-volume automotive manufacturers, are available for mass-production and not available through distributors. Access to InfoADAS SDK is through a TI representative.
For more information
- Watch the video on Informational ADAS.
- Read a blog on Informational ADAS.
- Keep up with the latest automotive happenings on Behind the Wheel blog.
- Join the TI E2E™ Community.
- Follow TI on Twitter and like TI on Facebook.
Texas Instruments drives automotive innovation
TI's state-of-the-art semiconductor products allow manufacturers and system suppliers to deliver world-class features to the automotive market. Our extensive automotive portfolio includes analog power management, interface and signal chain solutions, along with DLP® displays, ADAS and infotainment processors, Hercules™ TMS570 safety microcontrollers and wireless connectivity solutions. TI offers SafeTI™ parts designed to facilitate OEMs' compliance with the requirements of ISO 26262, as well as parts specifically designated as compliant with the AEC-Q100 and TS16949 standards, all with excellent product documentation. Visit TI's Automotive page or TI's E2E™ Behind the Wheel Blog to learn more about our commitment to automotive innovation.
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
All trademarks are the property of their respective owners.
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-drives-innovative-fusion-between-infotainment-and-informational-advanced-driver-assistance-systems-300094234.html
SOURCE Texas Instruments