TI makes developing 1080p pico display applications fast and easy with the DLP® LightCrafter™ Display 4710 evaluation module and robust ecosystem

Evaluation module, optical modules and reference designs help developers quickly incorporate bright, efficient full-HD projection in compact electronics

11 JUN 2015 | Uncategorized

DALLAS, June 11, 2015 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced the availability of the TI DLP LightCrafter Display 4710 evaluation module (EVM), a new developer tool that allows quick assessment of the DLP Pico™ 0.47-inch TRP Full-HD 1080p display chipset. Example applications include digital signage, mobile projectors (battery and AC-powered), screenless TVs, control panels, interactive displays, and wearables such as head-mounted displays (HMD). The EVM is now available for purchase through TI.com. For more information, see www.ti.com/4710evm.

TI DLP LightCrafter Display 4710 evaluation module

Key features and benefits of the DLP LightCrafter Display 4710 EVM:

  • Rapid assessment of the smallest DLP Full-HD chipset – the 0.47-inch TRP Full-HD 1080p chipset – capable of generating bright, power-efficient full-HD displays1 from small-form-factor electronics.
  • Mini High Definition Multimedia Interface (HDMI) offers plug-and-play functionality with various computing devices.
  • A simple-to-use micro-USB-based graphical user interface (GUI) allows for real-time chipset evaluation to assess features and peripherals.
  • Equipped with a production-quality optical engine to speed the product development cycle.

To help developers accelerate the incorporation of the 0.47-inch TRP Full-HD 1080p chipset in their application, a new TI Designs reference design, Full-HD Projection Display using DLP Pico technology , is now available for download, consisting of a system block diagram, schematics, board design files, test data and optical engine specifications.

To further accelerate developers' ability to bring their innovative products to market, TI maintains the most extensive ecosystem of pico optical engine manufacturers in the industry, eliminating the need for developers to have their own optics expertise. For more details, please contact a member of the DLP ecosystem.

Availability and package
The DLP LightCrafter Display 4710 EVM is available for purchase through TI.com. The chipset contained in this EVM includes the DLP4710 digital micromirror device. Other components in the chipset are the DLPC3439, available in a 201-pin very fine ball grid array (VFBGA) package; and the DLPA3005, offered in a 100-pin thermally enhanced thin quad flat pack (HTQFP) package.

Find out more:

About Texas Instruments DLP Products
Since 1996, award-winning TI DLP technology has powered the world's top display devices to deliver high-resolution images rich with color, contrast, clarity and brightness for a wide range of applications, including industrial, automotive, medical and consumer market segments. DLP technology is being used in movie theatres (DLP Cinema® products) and large-scale, professional venues and conference rooms, classrooms and home theaters. With mobile devices enabled by DLP® Pico™ technology, users have the ability to display images from the palm of their hand. Every DLP chipset features an array of microscopic mirrors that switch on and off up to 10,000 times per second. To learn more, please visit www.ti.com/dlp or follow TI DLP technology on Twitter at @TI_DLP.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
DLP and DLP Cinema are registered trademarks, and DLP Pico, LightCrafter, and TI E2E are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

1 The TI DLP4710 digital micromirror device incorporates 2,073,600 micromirrors (1080p resolution) within a 0.47-inch array diagonal, whereas the DLP4500 incorporates 1,024,000 micromirrors (WXGA resolution) within a 0.45-inch array diagonal.

TI DLP4710 digital micromirror device

Photo - http://photos.prnewswire.com/prnh/20150610/222240
Photo - http://photos.prnewswire.com/prnh/20150610/222239

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-makes-developing-1080p-pico-display-applications-fast-and-easy-with-the-dlp-lightcrafter-display-4710-evaluation-module-and-robust-ecosystem-300097405.html

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.