TI introduces industry's first industrial drive control system-on-chip (SoC) to support digital and analog position sensors

New C2000™ Delfino™ MCUs and DesignDRIVE Position Manager technology eliminate challenges of interfacing with position sensors in industrial servo and AC inverter drives

19 NOV 2015 | Uncategorized

HOUSTON, Nov. 19, 2015 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today announced the industry's first on-chip solution supporting both analog and digital position sensors. The new TMS320F28379D and TMS320F28379S microcontrollers (MCUs) are an expansion to TI's C2000™ Delfino™ MCU portfolio and, when combined with DesignDRIVE Position Manager technology, enable simple interfacing to position sensors. This solution improves system performance by completing the decode tasks on-chip and reducing the communication latency, enabling faster control loop performance. In addition, it allows developers to decrease system cost by reducing the board area required in FPGA or ASIC-based solutions. Position Manager gives developers access to the base functionality needed to interface to EnDat2.2, BiSS-C, Resolver and SIN/COS sensors, saving time in development, support and testing. Based on the real-time control architecture of TI's C2000 MCUs, the DesignDRIVE platform is ideal for the development of industrial inverter and servo drives used in robotics, computer numerical control machinery (CNC), elevators, materials conveyance, transportation and other industrial manufacturing applications.

New C2000(TM) Delfino(TM) MCUs and DesignDRIVE Position Manager technology eliminate challenges of interfacing with position sensors in industrial servo and AC inverter drives

Eliminate a complex stage of the industrial drives development cycle
DesignDRIVE is a single hardware and software platform that makes it easy for engineers to develop and evaluate solutions for a variety of industrial drive and servo topologies. Position Manager, a new technology within DesignDRIVE, allows developers to interface easily with digital and analog position sensors. The TMS320F28379D and TMS320F28379S MCUs are the first MCUs within the C2000 portfolio to support the Position Manager technology on-chip. As a key part of DesignDRIVE solutions, Position Manager allows industrial drives system designers to eliminate the engineering effort needed to develop, support and maintain the FGPAs or ASICs required to connect to these sensors today.

Solving position sensor interface compatibility challenges
TI's Position Manager technology is compatible with both digital and analog position sensors, which allows a single C2000 Delfino MCU the flexibility to support multiple sensor types. This includes EnDat 2.2, BiSS-C, Resolver, SIN/COS and incremental encoders including Clockwise/Counterclockwise protocols (CW/CCW). Texas Instruments is the only semiconductor vendor that supports both digital and analog position sensors for industrial applications. TI worked with HEIDENHAIN, a leading developer of position sensors, to test this on-chip solution to ensure compatibility. "We approve of Texas Instruments' successful implementation and testing of Position Manager to our EnDat specifications," said Herbert Reiter, HEIDENHAIN's Senior Product Manager "and we look forward to working with TI as they enable new EnDat capabilities for our customers."

Get started quickly with integrated support:

  • The C2000 DesignDRIVE development kit offers an easy path to begin exploring a wide variety of motor drive topologies, as well as easy expansion to develop with real-time Ethernet communications and functional safety topologies, enabling more comprehensive, integrated system solutions.
  • DesignDRIVE is supported by TI's C2000 controlSUITE™ package and includes specific examples of vector control of motors, incorporating current, speed and position loops, to help developers jumpstart their evaluation and development.
  • In addition, users can download TI's Code Composer Studio™ integrated development environment (IDE), providing code generation and debugging capabilities.
  • For Model-Based Design, TI's C2000 F28379D and F28379S MCUs are compatible with F28377D and F28377S, which are now supported by Mathworks' MATLAB®, Simulink® and Embedded Coder®.
  • Users can download reference interface and power supply designs for motor drives to either use immediately or modify to their specific needs.

In addition to using C2000 MCUs and DesignDRIVE technology, developers can integrate TI's new ISO5852S family of reinforced isolated gate drivers when developing industrial drive power stages. This family delivers the industry's highest working voltages of up to 1.5 kVrms, the industry's highest common mode transient immunity (CMTI) of 100 kV/μs minimum, and precision timing to efficiently drive high-voltage and fast switching insulated gate bipolar transistor (IGBT) and silicon carbide (SiC) power switches. Pricing for the new family starts at US$2.15 in 1,000-unit quantities (1ku).

Pricing and availability
The TMS320F28379D and TMS320F28379S MCUs are available for immediate sampling starting at $17.20 USD per 1 ku. Begin evaluating a diverse range of industrial drive designs today with TI's DesignDRIVE Kit (TMDXIDDK379D), which includes both the hardware and software for $999 and are available via the TI Store and authorized distributors. To further ease development, customers can download the Position Manager technology from the DesignDRIVE page on TI.com.

For more information:

Innovation is at the core of TI MCUs
Beginning with the foundation of leading process technology and adding unique system architecture, intellectual property and real-world system expertise, TI continues its 20+ years of MCU innovation with low-power and performance MCUs. With unique products for ultra-low power, low-power performance and security communications, to real-time control, control and automation, and safety, designers can accelerate time to market with TI's ecosystem of tools, software, wireless connectivity solutions, extensive Design Network offerings and technical support.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
C2000, Delfino, controlSUITE, Code Composer Studio and TI E2E are trademarks of Texas Instruments Incorporated. All registered trademarks and other trademarks belong to their respective owners.

Photo - http://photos.prnewswire.com/prnh/20151118/289010-INFO 

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-introduces-industrys-first-industrial-drive-control-system-on-chip-soc-to-support-digital-and-analog-position-sensors-300181391.html

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.