Spinning motors just got simpler with TI's latest stepper technologies

AutoTune™ technology dynamically tunes motors, and integrated current sensing saves 20 percent board space

11 JAN 2016 | Uncategorized

DALLAS, Jan. 11, 2016 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today enhanced its high-performance stepper motor-driver family with three new devices for 24-V stepper motors. Two devices offer TI's patented AutoTune™ technology to eliminate stepper motor tuning and two integrate current sensing to support differentiated 3D printers, robotics, factory automation equipment, currency-counting machines and more. Learn more or order samples at www.ti.com/drv8880-pr.

Spinning motors just got simpler with TI's latest stepper technologies

AutoTune technology on the DRV8880 and DRV8881 devices eliminates the time-consuming, iterative process of manual tuning, saving weeks or even months of design time. This on-chip intelligence dynamically monitors the motor's performance under varied conditions over its lifetime and adjusts decay settings appropriately. This functionality makes it possible to develop motors that run quietly and efficiently despite changes in motor properties, supply voltage, load and torque.

For motor systems that do not require the stability and longevity benefits of AutoTune technology, designers can take advantage of the new DRV8885 bipolar stepper motor driver with integrated current sensing. TI incorporates a unique technology that eliminates two external sense resistors to accurately regulate the current to the motor, saving up to 20 percent board space and simplifying routing compared to competing devices. Learn more or order samples at www.ti.com/drv8885-pr.

Other key features of the new stepper motor drivers are in the table below.

 

Device

Feature

Control interface

Current capacity

On-chip microstepping

DRV8880

AutoTune

Step/Direction

2.0 A full scale

(maximum drive current)

Yes; up to 1/16.

DRV8881

AutoTune

Phase/enable

2.0 A full scale

(maximum drive current)

No; external control allows for higher microstepping levels.

DRV8885

Integrated current sensing

Step/Direction

1.5 A full scale

(maximum drive current)

Yes; up to 1/16.

 

DRV8884

Integrated current sensing

Step/Direction

1 A full scale (maximum drive current)

Yes; up to 1/16.

 

Tools and support
Designers can speed evaluation and design with the new stepper-motor drivers using the DRV8880EVM, DRV8881EEVM (for phase/enable interface), DRV8881PEVM (for PWM interface) and DRV8885EVM evaluation modules (EVMs). Each EVM features an onboard MSP430TM microcontroller, giving designers a cost-effective platform that speeds development and time to market. Each is available for purchase at US$49 via the TI store and authorized distributors.

To support stepper-motor challenges, designers can search for solutions, ask questions, and share knowledge with fellow engineers and TI experts on the TI E2E Community Motor Driver forum.

Pricing and availability
The DRV8880 and DRV8881 are available now in 28-pin very thin quad flat no-lead (WQFN) and heat-sink thin-shrink small-outline package (HTSSOP) types. Pricing in 1,000-unit quantities starts at US$1.92 for the DRV8880 and US$1.60 for the DRV8881.

The DRV8885 is available now in a 24-pin HTSSOP package. Pricing in 1,000-unit quantities starts at US$1.50. The DRV8884 will be available soon in a 24-pin HTSSOP package. Pricing in 1,000 quantities starts at US$1.30.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
AutoTune, MSP430 and TI E2E are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

Photo - http://photos.prnewswire.com/prnh/20160108/320414

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/spinning-motors-just-got-simpler-with-tis-latest-stepper-technologies-300201698.html

SOURCE Texas Instruments (TI)

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.