TI drives high-voltage batteries with industry's first 100-V high-side FET driver

Unprecedented flexibility and power protection for advanced industrial battery applications

1 FEB 2016 | Uncategorized

DALLAS, Feb. 1, 2016 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced the first single-chip 100-V high-side FET driver for high-power lithium-ion battery applications, delivering advanced power protection and control. The bq76200 high-voltage solution efficiently drives high-side N-channel charge and discharge FETs in batteries commonly used in energy storage systems and motor-driven applications, including drones, power tools, e-bikes and more. For more details, see www.ti.com/bq76200-pr.

TI drives high-voltage batteries with industry's first 100-V high-side FET driver

Compared to typical 50-V low-side FET driver solutions, the 100-V high-side FET driver provides greater protection against possible inductive transient events in motor-driven applications, which can cause battery voltages to jump as much as 200 percent above normal. The bq76200 also helps maintain constant battery monitoring and enhanced system diagnostics – even when charging and discharging is disabled.

Key features and benefits of the bq76200:

  • Versatile supply voltage range: Compatible with a variety of battery architectures, capacities and voltage ranges from 8-V to 75-V, with an absolute maximum of 100-V.
  • Advanced-protection FET control: The fast-switching feature minimizes fault response time and disables the discharge FET if a battery has been severely discharged.
  • Quick development time and reduced overhead: The adaptable driver works with small to large power FET arrays by simply scaling the charge-pump capacitor, reducing engineering overhead and speeding development time.
  • High integration and small package size: The bq76200 integrates a high-voltage charge pump and dual FET drivers into one 5-mm by 4.4-mm by 1-mm thin shrink small outline package (TSSOP).

The bq76200 can be used in conjunction with the bq76940 battery-monitoring family, allowing for the application to move to a high-side FET drive and ensure that communication is always possible. The bq76200 can also drive TI's CSD19531Q5A 100-V NexFET™ power MOSFET as showcased in the bq76200 evaluation module.

Pricing and availability

The bq76200 is available now in the TI store and through the company's authorized distribution network. The driver is packaged in a 16-pin TSSOP and is priced at US$1.69 in 1,000-unit quantities.

Find out more about TI's battery-management solutions :

About Texas Instruments

Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks

WEBENCH is a registered trademark and TI E2E and NexFET are trademarks of Texas Instruments. All other trademarks belong to their respective owners.

Photo - http://photos.prnewswire.com/prnh/20160131/327780

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-drives-high-voltage-batteries-with-industrys-first-100-v-high-side-fet-driver-300212674.html

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.