New family of Texas Instruments SoCs drives down cost of multi-protocol industrial Ethernet communication

Sitara™ AMIC110 system on chip (SoC) simplifies industrial Ethernet communication and provides design versatility by supporting more than 10 standards

6 JUN 2017 | Uncategorized

DALLAS, June 6, 2017 /PRNewswire/ -- Cost-optimized industrial Ethernet communication is now attainable with the newly announced family of Sitara™ AMIC SoCs from Texas Instruments (TI) (NASDAQ: TXN). The AMIC110 SoC is a multiprotocol industrial communication processor that provides a ready-to-use solution supporting more than 10 industrial Ethernet and fieldbus communication standards. The device leverages TI's unified software platform, Processor SDK, and the programmability of TI's industrial communications subsystem (PRU-ICSS) for industrial communication support in factory automation and control applications. For more information, see www.ti.com/amic110-pr.    

New family of TI SoCs drives down cost of multi-protocol industrial Ethernet communication by supporting more than 10 standards

TI's new Sitara AMIC110 SoC helps developers convert existing non-networked designs such as motor drives to networked systems by adding industrial Ethernet. Unlike application-specific integrated circuits (ASICs), which may only support a single industrial Ethernet standard, AMIC110 SoC's programmable real-time unit (PRU-ICSS) supports many different protocols including EtherCAT, Profinet, Ethernet/IP, PROFIBUS master and slave, HSR, PRP, POWERLINK, SERCOS III, CANopen and more are in development. As the market moves to Industry 4.0, a programmable solution opens the door for designs to support more standards with no or minimal hardware changes.

Built on the industry-proven Sitara processor platform that features flexible peripherals, industrial temperature ranges and unified software support, the AMIC110 SoC was developed for industrial designers. The Sitara AMIC110 SoC can serve as a companion communication device to a microcontroller (MCU) such as TI's C2000™ MCU, for connected drive applications. By harnessing the strengths of C2000 MCU LaunchPad™ development kit and the AMIC110 industrial communication engine (ICE) development board, developers can create a highly integrated and scalable Industry 4.0-ready solution. Jump-start your design with the AMIC110 SoC by downloading the EtherCAT Slave and Multiprotocol Industrial Ethernet Reference Design. In addition to the AMIC110, this reference design also showcases the DP83822 PHY device that is well suited for Industrial Ethernet applications.

Pricing and availability
The AMIC110 SoC is available now through the TI store and authorized distributors at US$6.00 in 1,000-unit quantities.

Learn more about TI's cost-optimized and versatile Sitara AMIC110 SoCs

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping approximately 100,000 customers transform the future, today. Learn more at www.ti.com

Trademarks
C2000, LaunchPad and Sitara are trademarks of Texas Instruments. All other trademarks belong to their respective owners.

 

Texas Instruments Logo. (PRNewsFoto/Texas Instruments Incorporated)

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/new-family-of-texas-instruments-socs-drives-down-cost-of-multi-protocol-industrial-ethernet-communication-300467588.html

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.