Slash system power usage with TI's new fully integrated switch and sensor monitors

Cut board space and increase system protection in automotive and industrial applications with new multi-switch detection interface devices

10 OCT 2017 | Uncategorized

DALLAS, Oct. 10, 2017 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced two multi-switch detection interface (MSDI) devices that consume up to 98 percent less system power than conventional discrete solutions. The TIC12400 and TIC12400-Q1 are the first switch and sensor monitors that directly interface with resistor-coded switches. For more information, see www.ti.com/TIC12400Q1-pr.

Texas Instruments today introduced two multi-switch detection interface (MSDI) devices that consume up to 98 percent less system power than conventional discrete solutions.

Manufacturers, especially automotive manufacturers, are challenged to integrate more functionality while saving power and space. The TIC12400 and TIC12400-Q1 can alleviate this challenge by natively monitoring the inputs and decoding the resistor path of as many as 54 switches in one device, offloading the signal decoding task from the processor. Additionally, by directly monitoring and providing built-in diagnostics for 24 channel inputs, the devices' polling sequence architecture reduces the system microcontroller active time, significantly cutting system power usage for applications including automotive body electronics and factory and building automation equipment.

Key features and benefits of the TIC12400-Q1

  • 98 percent lower system power: Designers can reduce system power consumption from milliamps to microamps in applications that need high efficiency. On-device monitoring allows the microcontroller to go into a low-power sleep mode and use less power when idle, which is essential for applications like automotive start/stop or when a car is parked for extended periods of time.
  • Reduced complexity in a 60 percent smaller footprint: Eliminating up to 120 discrete components, the TIC12400-Q1 features an input-sharing and matrix mode that helps monitor 54 switches and sensors. The highly integrated device also includes adjustable wetting currents, timing controls, thresholds and built-in redundant circuitry for protection, which increases system-level reliability by reducing potential points of failure.
  • Robust, reliable system protection with simplified board layout: Integrated electrostatic discharge (ESD) protection and self-diagnostic features reduce external protection components. The new devices meet International Organization for Standardization (ISO) 10605 ±8-kV ESD protection requirements, preventing potential fault events from damaging internal circuitry. The fully configurable devices independently monitor and protect 24 inputs, providing more headroom for the host microcontroller to perform other functions.

Tools and support to speed design
The TIC12400 evaluation module (TIC12400EVM-KIT) enables designers to quickly and easily evaluate the new device's capabilities. It is available from the TI store for US$199.00.

Designers of automotive body control modules can decrease system cost and vehicle weight by leveraging the new device to create a smarter, more centralized architecture, reducing the number and overall weight of wires going into the harness. Explore how the TIC12400-Q1 can decode high-voltage switch inputs in the Automotive Multi-Switch Interface Reference Design.

Package, availability and pricing
The TIC12400-Q1, TIC12400 and TIC10024-Q1 are available in volume today through the TI store and authorized distributors. System designers who don't require high-volume input monitoring can select the TIC10024-Q1 to simplify the configuration for managing digital-only inputs. All three devices come in a 9.7-mm-by-4.4-mm thin-shrink small outline package (TSSOP). Features and pricing are listed in the following table:

Key features

TIC12400-Q1

Datasheet

TIC12400

Datasheet

TIC10024-Q1

Datasheet

Number of inputs

 

24 (analog and digital)

24 (analog and digital)

24 (digital only)

Input sharing & matrix mode features

Yes; up to 54 switch/sensor inputs

Yes; up to 54 switch/sensor inputs

No

1,000-unit price (USD)

$1.30

$1.10

$0.98

The TIC12400-Q1 and TIC10024-Q1 are the latest innovations in TI's complete interface portfolio that provides efficient, robust and reliable data communication for any application.

Learn more about TI's interface portfolio

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping approximately 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
TI E2E is a trademark of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.

 

Texas Instruments Logo. (PRNewsFoto/Texas Instruments Incorporated)

View original content with multimedia:http://www.prnewswire.com/news-releases/slash-system-power-usage-with-tis-new-fully-integrated-switch-and-sensor-monitors-300533483.html

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.