TI broadens 4K UHD display possibilities with newly expanded portfolio of DLP® Products

New DLP 4K UHD chipsets enable stunning display products capable of delivering accurate, detailed images across a variety of applications

5 DEC 2017 | Uncategorized

DALLAS, Dec. 5, 2017 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) is pushing the boundaries of 4K ultra-high definition (UHD) technology with an expanded family of chipsets to bring 4K UHD technology to new applications. Building on the introduction of the DLP660TE chipset, the first affordable 4K UHD offering in the industry, the portfolio now includes two smaller chipsets, the DLP470TE and DLP470TP, to expand the sharp image capabilities of 4K UHD into a broader range of end equipment.

DLP470TP, DLP470TE & DLP660TE

Developers can now design DLP 4K UHD technology into a variety of end products such as laser TVs, mobile smart TVs, digital signage displays, smart home displays, pico projectors, business and education projectors, and more. The chipsets span a wide range of power, size, brightness and performance levels to help designers achieve any 4K UHD end-equipment objective. For more information about display offerings in TI's DLP Products portfolio, see http://www.ti.com/DLP4kExpansion-pr.

Each DLP 4K UHD chipset exceeds the Consumer Technology Association (CTA) definition for 4K UHD technology, displaying over 8 million pixels on the screen.

Key features and benefits of the chipsets

  • The DLP470TP is the most compact 4K UHD solution from DLP Products, and is optimized for size and power. Measuring 17 mm by 24.5 mm and supporting brightness levels up to 1,500 lumens, the DLP470TP can deliver 4K UHD quality to equipment such as mobile smart TVs and pico projectors.
  • The DLP470TE is optimized for projectors needing over 1,500 lumens. This chipset is in a larger package, 22 mm by 32 mm, which enables it to withstand the heat generated by brightness levels up to 4,000 lumens.
  • The DLP660TE is the most powerful of the three 4K UHD chipsets. This digital micromirror device (DMD) is designed to enable projection applications up to 5,000 lumens.

TI collaborates with the most extensive ecosystem of optical engine manufacturers in the industry. This offers developers a path to production-ready optical engines, reducing design time and helping companies get their innovative products to market faster. To learn more, please visit the optical engine manufacturer page.

Availability
Developers can get started immediately with the DLP660TE which is available now in the TI store and through authorized distributors. The DLP470TE and DLP470TP will be in production in early 2018.

Learn more about the DLP Products 4K UHD portfolio

About Texas Instruments DLP Products
Since 1996, award-winning TI DLP technology has powered the world's top display devices to deliver high-resolution images rich with color, contrast, clarity and brightness for a wide range of applications, including industrial, automotive, medical and consumer market segments. DLP technology is used in movie theatres (DLP Cinema® products) and large-scale, professional venues and conference rooms, classrooms and home theaters. With mobile devices enabled by DLP Pico technology, users have the ability to display images from the palm of their hand. Every DLP chipset features an array of microscopic mirrors that switch on and off up to 10,000 times per second. To learn more, please visit www.ti.com/dlp or follow TI DLP technology on Twitter at @TI_DLP.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping approximately 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
DLP and DLP Cinema are registered trademarks and Pico are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

 

Texas Instruments Logo. (PRNewsFoto/Texas Instruments Incorporated)

View original content with multimedia:http://www.prnewswire.com/news-releases/ti-broadens-4k-uhd-display-possibilities-with-newly-expanded-portfolio-of-dlp-products-300565861.html

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized
Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.