Industry's first zero-drift, nanopower amplifier combines ultra-high precision with the lowest power consumption

TI delivers the most precise nanopower op amp, reducing system power and maximizing battery life in precision IoT, industrial and personal electronics applications

6 DEC 2017 | Uncategorized

DALLAS, Dec. 6, 2017 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced the first operational amplifier (op amp) to combine ultra-high precision with the industry's lowest supply current. With exceptional power-to-precision performance, the LPV821 zero-drift, nanopower op amp enables engineers to attain the highest DC precision, while consuming 60 percent less power than competitive zero-drift devices. The LPV821 is designed for use in precision applications such as wireless sensing nodes, home and factory automation equipment, and portable electronics. For more information, see www.TI.com/LPV821-pr.

TI delivers the most precise nanopower op amp, reducing system power and maximizing battery life in precision IoT, industrial and personal electronics applications

The LPV821 op amp is the newest device in TI's low-power amplifier portfolio, which enables engineers to design lighter, smaller and more portable applications with lower-capacity batteries and longer system lifetimes.

Key features and benefits of the LPV821 op amp

  • Exceptional power-to-precision performance: Consuming only nanoamps of supply current, while providing the high-precision benefits of optimized offset, drift and 1/f noise (flicker noise), the LPV821 is extremely beneficial for applications where both precision and low power are essential system needs, including industrial gas detectors, field transmitters and battery packs.
  • Sixty percent lower power consumption: With best-in-class supply current of 650 nA, the LPV821 extends battery lifetimes and enables lower power budgets in precision systems than competitive zero-drift devices.
  • High DC precision: TI's zero-drift technology delivers a low initial offset of 10 µV and an offset drift of 0.02 µV/°C, eliminating temperature drift and flicker noise, and enabling engineers to attain the highest DC precision and dynamic error correction. Additionally, self-calibration technology helps engineers save system development cost and speed time to market.
  • No duty cycling: Nanopower consumption enables always-on applications such as continuous and blood glucose monitoring, and other electrochemical cell applications. Additionally, the low supply current decreases the external circuitry required to turn the amplifier on and off.
  • High-impedance sensor operation: An input bias current of 7 pA and low flicker noise at 3.9 µVp-p enables operation with high-impedance sensors, delivering more accurate measurements in precision systems.

Engineers can pair the LPV821 op amp with the TLV3691 nanopower comparator or ADS7142 nanopower analog-to-digital converter (ADC) to program a threshold that will automatically wake up a microcontroller (MCU) such as the CC1310 SimpleLink™ Sub-1 GHz MCU, further reducing system power consumption.

Tools and support to speed design
Designers can download the TINA-TI™ SPICE model to simulate their designs and predict circuit behavior when using the LPV821 op amp. Engineers can also jump-start gas-sensing system designs using the LPV821 op amp with the Always-On Low-Power Gas Sensing with 10+ Year Coin Cell Battery Life Reference Design and Micropower Electrochemical Gas Sensor Amplifier Reference Design.

Package, availability and pricing
Pre-production samples of the LPV821 op amp are now available through the TI store and authorized distributors in a 5-pin small-outline transistor (SOT-23) package. Pricing starts at US$0.80 in 1,000-unit quantities.

Learn more from TI's amplifier experts

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping approximately 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
SimpleLink, TINA-TI and TI E2E are trademarks of Texas Instruments. All other trademarks belong to their respective owners.

 

Texas Instruments Logo. (PRNewsFoto/Texas Instruments Incorporated)

View original content with multimedia:http://www.prnewswire.com/news-releases/industrys-first-zero-drift-nanopower-amplifier-combines-ultra-high-precision-with-the-lowest-power-consumption-300567037.html

SOURCE Texas Instruments Incorporated

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.