Industry's smallest linear thermistors help engineers reach new thermal limits

TI's new temperature sensors offer 50% higher accuracy, high sensitivity and single-point calibration

17 FEB 2020 | Products and technologies

DALLAS, Feb. 17, 2020 /PRNewswire/ -- Texas Instruments (TI) (Nasdaq: TXN) today expanded its temperature sensing portfolio to include linear thermistors that deliver up to 50% higher accuracy than negative temperature coefficient (NTC) thermistors. The higher accuracy of TI's thermistors enables operation closer to the thermal limits of the other components and the overall system, helping engineers maximize performance while reducing bill-of-materials (BOM) and total solution cost. For more information, see www.ti.com/thermistors-pr.

TI’s new temperature sensors offer 50% higher accuracy, high sensitivity and single-point calibration.

NTC thermistors are widely used due to their low price; however, they present several challenges to design engineers, including degraded performance at temperature extremes and complex calibration requirements, which increases design time. TI's new linear thermistors are available at a similar price while providing significantly more value – most notably minimizing design time, reducing component count and increasing system performance.

Extend system performance and reliability
TI's new thermistors deliver reliable, highly accurate thermal measurements, particularly at temperatures above 80°C. This is especially important for industrial, automotive and consumer applications where precise, real-time temperature readings are fundamental to system performance and protection. To learn more about the differences between NTCs and TI's linear thermistors, read the white paper, "Temperature sensing with thermistors."

NTC thermistors provide less accurate temperature readings due to their low sensitivity and high resistance tolerance at temperature extremes. To compensate for these challenges, many engineers calibrate at three points across the temperature range or use multiple thermistors to monitor different temperature ranges. These approaches can still produce unreliable temperature readings, which can require systems to shut down before reaching their true thermal limit. The linearity and high accuracy of TI's thermistors enable single-point calibration, which maximizes system performance and simplifies design.

TI's thermistors also offer very low typical drift of 0.5% to improve the reliability of temperature measurements, enabling designers to boost system performance while maintaining safe operation. Engineers can use TI's thermistor design tool, available on the thermistor product pages and data sheets on TI.com, to quickly and easily calculate temperature resistance values and kick-start their design with example conversion methods and code.

Reduce system cost and size
By eliminating the need for additional linearization circuitry or redundant NTC thermistors, TI's thermistors help engineers simplify design, lower system cost and reduce printed circuit board (PCB) layout size by at least 33%, compared to NTC thermistors. In addition, TI's thermistors are one-tenth the size of similar silicon-based linear thermistors, with a low profile and small package area that enable placement closer to thermal hot spots for faster thermal response and more consistent temperature measurements.

Package, availability and pricing
TI's new thermistor portfolio, which includes the TMP61, TMP63 and TMP64, is available now through TI and authorized distributors with starting prices as low as US$0.05 in 1,000-unit quantities. The devices are offered in through-hole packaging and surface-mount 0402 and 0603 footprint options.

 

Product

Resistance

Package type

Buy now from TI

Evaluation module

 

TMP61

10 kΩ

0402 footprint

TMP61

TMP6EVM

 

0603 footprint

 

TO-92S

 

TMP61-Q1

10 kΩ

0402 footprint – Grade 1

TMP61-Q1

 

0603 footprint – Grade 1

 
 

TO-92S  – Grade 1

 
 

TO-92S – Grade 0

 
 

TMP63

100 kΩ

0402 footprint

TMP63

 

TMP63-Q1

100 kΩ

0402 footprint – Grade 1

TMP63-Q1

 

TMP64

47 kΩ

0402 footprint

TMP64

 

About Texas Instruments
From connected cars and intelligent homes to self-monitoring health devices and automated factories, Texas Instruments Incorporated (TI) (Nasdaq: TXN) products are at work in virtually every type of electronic system. With operations in more than 30 countries, we engineer, manufacture, test and sell analog and embedded semiconductor chips. Our employees, about 30,000 worldwide, are driven by core values of integrity, innovation and commitment, and work every day to shape the future of technology. Learn more at www.ti.com.

Trademarks
All registered trademarks and other trademarks belong to their respective owners.

 

 

Cision View original content to download multimedia:http://www.prnewswire.com/news-releases/industrys-smallest-linear-thermistors-help-engineers-reach-new-thermal-limits-301005487.html

SOURCE Texas Instruments

Related news releases

TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor
09 Jun 2026 | Products and technologies
TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor

Engineers can build safer, higher-performing electric vehicles and energy storage systems with TI's new BQ79826Z-Q1 battery monitor

TI unveils high-performance isolated power modules to advance power density in data centers and EVs
23 Mar 2026 | Products and technologies
TI unveils high-performance isolated power modules to advance power density in data centers and EVs

New power modules with proprietary IsoShield™ technology deliver industry-leading power density

TI unveils complete 800 VDC power architecture for future generation AI data centers with NVIDIA
16 Mar 2026 | Products and technologies
TI unveils complete 800 VDC power architecture for future generation AI data centers with NVIDIA

TI's complete power solution includes multiple breakthrough reference designs with industry-leading specification

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.