New portfolio of isolation devices from TI extends the lifetime of high-voltage applications to 40-plus years

19 SEP 2023 | Products and technologies

News highlights:

  • Improve signal integrity and reduce power consumption as much as 80% with pin-to-pin replacement to optocouplers.
  • New opto-emulators improve performance over end-product lifetimes with TI's proprietary SiO2-based isolation technology.

DALLAS , Sept. 19, 2023 /PRNewswire/ -- Texas Instruments (TI) (Nasdaq: TXN) today introduced its new opto-emulator portfolio of signal isolation semiconductors, designed to improve signal integrity, consume less power, and extend the lifetime of high-voltage industrial and automotive applications. TI's inaugural opto-emulators are pin-to-pin compatible with the industry's most common optocouplers, enabling seamless integration into existing designs while leveraging the unique benefits of silicon dioxide (SiO2)-based isolation technology. For more information, see TI.com/opto-emulators.

"Today's push for electrification, coupled with the intricacies of designing high-voltage systems, presents a need for engineers to increase the performance and lifetime of their products while ensuring the right level of isolation," said Tsedeniya Abraham, general manager of interface products at Texas Instruments. "Our new portfolio of opto-emulators not only addresses the growing need for reliable and affordable isolation, but also exemplifies our commitment to investing in high-voltage technologies."

Increase reliability with TI's SiO2-based isolation
Optocouplers, which integrate an LED to isolate the signal, have historically been a common choice among engineers. However, optocouplers typically require upfront overdesign to compensate for the inevitable aging effects of LEDs. TI's opto-emulators eliminate the need for overdesign by using SiO2 for the isolation barrier, removing the effects of LED aging altogether. With a high dielectric strength of 500 VRMS/µm, TI's SiO2 isolation barrier enables the new portfolio of devices to protect end-product designs for more than 40 years. Opto-emulators also provide isolation protection as high as 3,750 VRMS, while reducing power consumption by as much as 80%.

Additionally, the portfolio is able to withstand wide operating temperature ranges from –55°C to 125°C, while providing common-mode transient immunity up to 10 times higher than optocouplers. To learn more about the benefits of TI's new opto-emulators, read the technical article, "Opto-Emulators Explained: Why You Should Upgrade Your Optocoupler Technology."

TI's new opto-emulator portfolio builds on the company's commitment to helping engineers unlock the power of high voltage. To learn more, see TI.com/highvoltage.

Package, availability and pricing
Preproduction quantities of opto-emulator products are available now at TI.com/opto-emulators.

  • Package options as small as 4.8 mm by 3.5 mm.
  • Evaluation modules start at US$19.00.
  • Multiple payment and shipping options available.
  • Automotive versions of opto-emulator products are expected to be available in 2024.

About Texas Instruments
Texas Instruments Incorporated (Nasdaq: TXN) is a global semiconductor company that designs, manufactures, tests and sells analog and embedded processing chips for markets such as industrial, automotive, personal electronics, communications equipment and enterprise systems. Our passion to create a better world by making electronics more affordable through semiconductors is alive today, as each generation of innovation builds upon the last to make our technology smaller, more efficient, more reliable and more affordable – making it possible for semiconductors to go into electronics everywhere. We think of this as Engineering Progress. It's what we do and have been doing for decades. Learn more at TI.com.

Trademarks
All registered trademarks and other trademarks belong to their respective owners.

 

Cision View original content to download multimedia:https://www.prnewswire.com/news-releases/new-portfolio-of-isolation-devices-from-ti-extends-the-lifetime-of-high-voltage-applications-to-40-plus-years-301931276.html

SOURCE Texas Instruments

Related news releases

TI debuts new approach to current sensing for unprecedented accuracy in HEV and EV traction inverter designs
25 Aug 2026 | Products and technologies
TI debuts new approach to current sensing for unprecedented accuracy in HEV and EV traction inverter designs

Innovative multiaxial sensing architecture achieves 20 times greater accuracy than single-axis, coreless alternatives, driving more compact and efficient traction inverter systems

TI advances next-generation industrial systems with the first commercially available CAN XL transceiver
12 Aug 2026 | Products and technologies
TI advances next-generation industrial systems with the first commercially available CAN XL transceiver

New TCAN6062 CAN XL transceiver delivers the highest bandwidth and largest payload of any CAN-based network while preserving the advantages of proven CAN protocols

TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor
09 Jun 2026 | Products and technologies
TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor

Engineers can build safer, higher-performing electric vehicles and energy storage systems with TI's new BQ79826Z-Q1 battery monitor

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.