TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor

9 JUN 2026 | Products and technologies

 Engineers can build safer, higher-performing electric vehicles and energy storage systems with TI's new BQ79826Z-Q1 battery monitor

News highlights:

  • The industry's first 26-cells-in-series channel battery monitor delivers best-in-class sensing accuracy, reducing system costs by supporting more cells per device than competing solutions.
  • Integrated smart EIS engine enables early warning of thermal runaway from inside battery cells, helping ensure safety in EVs and ESSs.
  • Designed to help engineers create safer, higher-performing automotive and industrial applications, the BQ79826Z-Q1 is the latest addition to TI's portfolio of BMS devices.

DALLAS, June 9, 2026 /PRNewswire/ -- Texas Instruments (TI) (Nasdaq: TXN) today introduced the industry's highest-cell-count battery monitor with an integrated electrochemical impedance spectroscopy (EIS) engine, bringing predictive intelligence, comprehensive data and real-time diagnostics to battery monitoring in electric vehicles (EV) and energy storage system (ESS) applications.

TI’s new BQ79826Z-Q1 battery monitor enables increased safety and performance in EVs and ESSs.

The BQ79826Z-Q1 battery monitor enhances safety and extends battery life by detecting potential failures from within battery cells. The single chip delivers the highest-cell-count monitoring in its class, tracking up to 44% more channels than previous generations. With this increase in channels, the device significantly decreases the number of components required in a battery pack, reducing system complexity and cost without compromising reliability. TI is showcasing this innovation at the 2026 Power Conversion, Intelligent Motion Expo and Conference (PCIM), June 9-11, in Nuremberg, Germany.

"The electrification of transportation and the rapid expansion of energy storage are redefining what battery performance must deliver, and as a leader in battery management technology, TI is uniquely positioned to meet that challenge," said Wenjia Liu, vice president and general manager, battery management systems (BMS) at TI. "Our high-cell-count battery monitor with a built-in EIS engine helps 'shine a light' inside battery cells, delivering rich chemical-state data that enables systems' software to make informed, real-time decisions on safety and performance of the battery pack, allowing engineers to address the most critical challenges in battery management."

For more information, see ti.com/BQ79826Z-Q1.

Delivering safety and performance with EIS technology
Just as an electrocardiogram (EKG) monitors the heart, EIS monitors a battery. It delivers continuous, real-time insight that reveals the battery's health and warns of issues before they become critical. Integrated EIS technology enables the BQ78926Z-Q1 to detect fault conditions earlier – from inside the cells – helping maintain safety and notifying passengers of potential vehicle hazards such as thermal runaway.

These same benefits extend to ESSs, where reliable battery monitoring is critical to meeting the growing power demands of artificial intelligence data centers. As effective storage solutions become increasingly vital in the grid-to-gate ecosystem, EIS gives engineers real-time visibility into the state of charge and state of health of each battery cell, regardless of system size.

Maximizing efficiency with industry-leading cell count
The performance of an EV or ESS is fundamentally affected by the quality and efficiency of its batteries. The BQ79826Z-Q1 supports up to 26 cells per device, eight more than any competing solution, setting a new industry standard. Fewer monitoring devices means a lower bill of materials, simplified architecture and reduced board space requirements, translating to meaningful cost savings per channel without sacrificing quality or reliability.

When paired with the BQ79881-Q1 pack monitor and optional TI communications bridge, these devices create a powerful chipset that works across different module sizes, battery chemistries and mechanical designs, giving engineers the flexibility to design once and deploy everywhere. This scalability reduces engineering overhead and accelerates time to market for automotive and energy storage designers.

Calculating charge readings with the best-in-class accuracy
With a voltage accuracy of <2mV across a full temperature range of –40°C to +125°C, higher resolution analog-to-digital converters and ultra-low noise, the BQ78926Z-Q1 enables more accurate state-of-charge calculations, directly addressing one of the biggest concerns for EV drivers: range anxiety. Utilizing EIS technology, this device enables more accurate temperature and state-of-charge estimation, helping designers achieve longer battery life and faster charging without compromising battery health. With an EIS measurement time that is five times faster than previous solutions, this device delivers the highest functional safety voltage reading per cell. Compliance with Automotive Safety Integrity Level D and International Organization for Standardization 26262 gives designers a smarter, more efficient path to safer, longer-lasting batteries.

For more information on the BQ79826Z-Q1, see technical article "Enabling the next phase of battery intelligence."

Innovating what's next in power at PCIM 2026
Visitors to PCIM can see new products and solutions from TI that are enabling engineers to innovate what's next in power in Hall 7, Booth No. 652. The new BQ79826Z-Q1 battery monitor will be featured in an EIS-enabled BMS reference design, alongside other innovations such as an 11kW single-stage bidirectional onboard charger, a 50kVA solid-state transformer cell stack with Ethernet and Fast Serial Interface communication and short-circuit protection for silicon carbide power metal-oxide semiconductor field-effect transistors with technology from Flex.

For more information about TI at PCIM, see ti.com/pcim.

Availability

  • Preproduction quantities of the BQ79826Z-Q1 battery monitor with integrated EIS engine are now available on TI.com, with production quantities expected by the end of 2026.
  • To support designers, complete development support including evaluation modules and reference designs are available.

About Texas Instruments
Texas Instruments Incorporated (Nasdaq: TXN) is a global semiconductor company that designs, manufactures and sells analog and embedded processing chips for markets such as industrial, automotive, data center, personal electronics and communications equipment. At our core, we have a passion to create a better world by making electronics more affordable through semiconductors. This passion is alive today as each generation of innovation builds upon the last to make our technology more reliable, more affordable and lower power, making it possible for semiconductors to go into electronics everywhere. Learn more at TI.com.

SOURCE Texas Instruments

Related news releases

TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor
09 Jun 2026 | Products and technologies
TI brings intelligence to battery management systems with industry's highest-cell-count EIS-enabled battery monitor

Engineers can build safer, higher-performing electric vehicles and energy storage systems with TI's new BQ79826Z-Q1 battery monitor

TI unveils high-performance isolated power modules to advance power density in data centers and EVs
23 Mar 2026 | Products and technologies
TI unveils high-performance isolated power modules to advance power density in data centers and EVs

New power modules with proprietary IsoShield™ technology deliver industry-leading power density

TI unveils complete 800 VDC power architecture for future generation AI data centers with NVIDIA
16 Mar 2026 | Products and technologies
TI unveils complete 800 VDC power architecture for future generation AI data centers with NVIDIA

TI's complete power solution includes multiple breakthrough reference designs with industry-leading specification

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.