Home
Videobibliothek

Webinar: Develop a functionally safe signal chain application

00:00:12 | 07 OKT. 2021
 

ABOUT THIS WEBINAR

Factory automation has increased the need for functional safety in the industrial sector. Functional safety may be required across industrial applications such as factory automation and control systems. Functional safety is part of the overall safety of a system and depends on responding in a predictable manner to certain inputs or a failure state.

Note: Please note that this presentation uses an example signal-chain sub-system for a 4-20mA analog input module implementation where a FS 2-wire sensor transmitter is connected to the input. For instance, this configuration demonstrates how to measure relevant process data, such as temperature or the level of liquid in a tank within a functional safety application. However, this sub-system may also be integrated in other applications.

AGENDA

tbd

OUR PRESENTER

Lars Lotzenburger is a system engineer in the factory automation and control sector also certified on Functional Safety (IEC 61508). Lars works to support worldwide customers regarding functional safety and PLC I/O modules. He joined the industrial systems team in 2015 where he supported signal chain reference designs. Early in his career, Lars helped develop interface drivers for ADCs and DACs before helping create the powerline communication business in EMEA. Since joining Texas Instruments in 2002, he has worked in both the analog and digital world which has allowed him to better understand today's customer systems.

Ressourcen

  • arrow-right Training: Overview of Functional Safety at TI
  • download Understanding Functional Safety FIT Base Failure Rate Estimates per IEC 62380 and SN 29500 white paper
  • download Streaming functional safety certification in automotive and industrial white paper
  • arrow-right ADS1119