C64x+ TI Benchmark Routines Library Installation
(C) Copyright 2005 Texas Instruments Incorporated
All rights reserved worldwide.
-------------------------------------------------

CONTENTS
-------------
- ZIPFILE CONTENTS
- INSTALLATION INFORMATION
- CONTACTING TI


ZIPFILE CONTENTS
----------------------
C64x+TIBenchmarksRoutines_v100.exe - Contains the installation program for the C64x+ TI Benchmark Routines Library.
Readme.txt - This file.


INSTALLATION INFORMATION
-----------------------------------
To run the TI C64x+ TI Benchmark Routines Library Installation, follow the directions below:

Windows 98, Windows NT, Windows 2000, Windows XP
1. Unzip the C64x+TIBenchmarksRoutines_v100.exe file to a temp directory
2. Double Click the file to launch the Install Shield Wizard
3. Answer all remaining questions presented in Install Shield dialog boxes

NOTES: 
1) If you DO NOT accept the software license agreement the library WILL NOT be installed. 
2) The source code for the TI Benchmark Routines are available in this package. 
3) The default location to install the software is C:\CCStudio_v3.2\, which will install the code into C:\CCStudio_v3.2\c64plus\.  If the existing tools are not installed in the default location you need to know the correct location to complete the installation of the C64x+ TI Benchmark Routines Library.

PERFORMANCE INFORMATION
-----------------------
Please refer to the Readme.txt in the install directory for cycle count and code size data.