SBAS603B April 2013 – November 2020 ADS4449
PRODUCTION DATA
The device includes a mode where the contents of the internal registers can be read back, as shown in Figure 8-9. This readback mode can be useful as a diagnostic check to verify the serial interface communication between the external controller and ADC.
Note that the contents of register 00h cannot be read back because the register contains RESET and READOUT bits. When the READOUT bit is disabled, the SDOUT terminal is in a high-impedance state. If serial readout is not used, the SDOUT terminal must not be connected (must float).
SDOUT comes out at the SCLK rising edge with an approximate delay (tSD_DELAY) of 8 ns, as shown in Figure 8-10.