DLPS136 November 2018 DLP650LNIR
PRODUCTION DATA.
Operational DMD Temperature and Landed Duty Cycle interact to affect the useable life of the DMD, and this interaction can be exploited to reduce the impact that an asymmetrical Landed Duty Cycle has on the useable life of the DMD. This is quantified in the de-rating curve shown in Figure 2. The importance of this curve is that:
In practice, this curve specifies the Maximum Operating DMD Temperature at a given long-term average Landed Duty Cycle.