15 |
RESERVED |
R |
0x0 |
Reserved
|
14 |
LED_GPIO_POLARITY |
R/W |
0x1 |
GPIO LED polarity: Default depends on strap, non strap default Active High
0x0 = Active low
0x1 = Active high
|
13 |
LED_GPIO_DRV_VAL |
R/W |
0x0 |
If bit #12 is set, this is the value of GPIO LED
|
12 |
LED_GPIO_DRV_EN |
R/W |
0x0 |
Force value to LED_GPIO as per bit #13
0x0 = LED_GPIO is in normal operation mode
0x1 = Force the value of LED_GPIO
|
11 |
RESERVED |
R |
0x0 |
Reserved
|
10 |
LED_2_POLARITY |
R/W |
0x1 |
LED_2 polarity. Default depends on strap, non strap default Active High
0x0 = Active low
0x1 = Active high
|
9 |
LED_2_DRV_VAL |
R/W |
0x0 |
If bit #8 is set, this is the value of LED_2
|
8 |
LED_2_DRV_EN |
R/W |
0x0 |
Force value to LED_GPIO as per bit #9
0x0 = LED_2 is in normal operation mode
0x1 = Drive the value of LED_2
|
7 |
RESERVED |
R |
0x0 |
Reserved
|
6 |
LED_1_POLARITY |
R/W |
0x1 |
LED_1 polarity: Default depends on strap, non strap default Active High
0x0 = Active low
0x1 = Active high
|
5 |
LED_1_DRV_VAL |
R/W |
0x0 |
If bit #4 is set, this is the value of LED_1
|
4 |
LED_1_DRV_EN |
R/W |
0x0 |
Force value to LED_GPIO as per bit #5
0x0 = LED_1 is in normal operation mode
0x1 = Drive the value of LED_1
|
3 |
RESERVED |
R |
0x0 |
Reserved
|
2 |
LED_0_POLARITY |
R/W |
0x1 |
LED_0 polarity: Default depends on strap, non strap default Active High
0x0 = Active low
0x1 = Active high
|
1 |
LED_0_DRV_VAL |
R/W |
0x0 |
If bit #1 is set, this is the value of LED_0
|
0 |
LED_0_DRV_EN |
R/W |
0x0 |
Force value to LED_GPIO as per bit #1
0x0 = LED_0 is in normal operation mode
0x1 = Drive the value of LED_0
|