A minimum of four layers is required to accomplish
a low EMI PCB design (see Figure 8-15). Layer stacking must be in the following order (top-to-bottom): high-speed
signal layer, ground plane, power plane and low-frequency signal layer.
- Routing the high-speed traces on the top layer
avoids the use of vias (and the introduction of the inductances) and allows for
clean interconnects between the isolator and the transmitter and receiver
circuits of the data link.
- Placing a solid ground plane next to the high-speed signal layer establishes controlled impedance for transmission line interconnects and provides an excellent low-inductance path for the return current flow.
- Placing the power plane next to the ground plane
creates additional high-frequency bypass capacitance of approximately
100pF/inch2.
- Routing the slower speed control signals
on the bottom layer allows for greater flexibility as these signal links typically have
margin to tolerate discontinuities such as vias.
- A low-ESR ceramic bypass-capacitor must
be connected between the VCC and GND pins for both the supply. The recommended
capacitor value can range from 0.1μF to 10μF. The capacitor must have a voltage rating of
10V minimum and a X5R or X7R dielectric. The optimum placement of decap is closest to the
VCC and GND pins.
- The connections between the device D1 and
D2 pins and the transformer primary endings, and the connection of the device
VCC1 pin and the transformer center-tap must be as close as possible for
minimum trace inductance. And 10μF capacitor must be connected close to the transformer
center-tap pin. Length matching of D1 and D2 traces provide the best performance in
efficiency and EMI.
- The rectifier diodes must be Schottky
diodes with low forward voltage in the 10mA to 100mA current range to maximize
efficiency.
If an additional supply voltage plane or signal
layer is needed, add a second power or ground plane system to the stack to keep the
planes symmetrical. This design makes the stack mechanically stable and prevents
warping. Also the power and ground plane of each power system can be placed closer
together, thus increasing the high-frequency bypass capacitance significantly.
For detailed layout recommendations, refer to the Digital Isolator Design Guide.