A power supply input typically has a relatively
high source impedance at the switching frequency. Good-quality input capacitors are
necessary to limit the input ripple voltage. In general, the ripple current splits between
the input capacitors based on the relative impedance of the capacitors at the switching
frequency.
- Select the input capacitors with sufficient voltage and RMS ripple current ratings.
- Use Equation 40 to calculate the input capacitor RMS ripple current assuming a
worst-case duty-cycle operating point of 50%.
Equation 40.
- Use Equation 41 to find the required input capacitance.
Equation 41.
where
- ΔVIN is the input
peak-to-peak ripple voltage specification.
- RESR is the input
capacitor ESR.
- Recognizing the voltage coefficient of ceramic
capacitors, select two 10µF, 50V, X7R, 1210 ceramic input capacitors. Place these
capacitors adjacent to the power MOSFETs. See also Section 7.4.1.1.
- Use four 10nF, 50V, X7R, 0603 ceramic capacitors
near the high-side MOSFET to supply the high di/dt current during MOSFET switching
transitions. Such capacitors offer high self-resonant frequency (SRF) and low effective
impedance above 100MHz. The result is lower power loop parasitic inductance, thus
minimizing switch-node voltage overshoot and ringing for lower conducted and radiated EMI
signature. See also Section 7.4.1.