SNVSCF0 October 2024 LM65680-Q1
ADVANCE INFORMATION
The LM656x0-Q1 can have two behaviors while lightly loaded. One behavior, called auto mode operation, allows a seamless transition between normal current mode operation while heavily loaded and in highly-efficient light-load operation. The other behavior, called FPWM mode, maintains full frequency even when unloaded. Which mode the LM656x0-Q1 operates in depends on the SYNC/MODE pin. When SYNC/MODE is high, the part is in FPWM. When SYNC/MODE is low, the part is in PFM.
In auto mode, light-load operation is employed in the LM656x0-Q1 at load lower than approximately 1/10th of the rated maximum output current. Light-load operation employs two techniques to improve efficiency:
Note that while these two features operate together to create excellent light load behavior, these features operate independently of each other.