SNAS698C May 2020 – November 2022 LMK04832-SP
PRODUCTION DATA
Under the advanced tab of the Clock Architect, filtering of specific parts can be done using regular expressions in the Part Filter box. [LMK04832.*] will filter for only the LMK04832 device (without brackets). More detailed filters can be given such as the entire part name LMK04832_VCO0 to force an LMK04832 using VCO0 solution if one is available.