SLLSFX9A December 2024 – May 2025 MCF8316D
PRODUCTION DATA
Low-side braking mode is configured by setting MTR_STOP to 010b. When a motor stop command is received, the output speed is reduced to a value defined by BRAKE_SPEED_THRESHOLD prior to turning all low-side MOSFETs ON (see example Figure 7-56) for a time configured by MTR_STOP_BRK_TIME. If the motor speed is below BRAKE_SPEED_THRESHOLD prior to receiving stop command, then the MCF8316D transitions directly into the brake state. After applying the brake for MTR_STOP_BRK_TIME, the MCF8316D transitions into the Hi-Z state by turning OFF all MOSFETs.
The MCF8316D can also enter low-side braking through BRAKE pin input. When BRAKE pin is pulled to HIGH state, the output speed is reduced to a value defined by BRAKE_SPEED_THRESHOLD prior to turning all low-side MOSFETs ON. In this case, MCF8316D stays in low-side brake state till BRAKE pin changes to LOW state.