For best operational performance of the device,
use good PCB layout practices, including:
- Noise can propagate into analog circuitry through
the power pins of the circuit as a whole and the
op amp. Use bypass capacitors to reduce the
coupled noise by providing low-impedance power
sources local to the analog circuitry.
- Connect low-ESR, 0.1-µF ceramic bypass capacitors
between each supply pin and ground, placed as
close as possible to the device. A single bypass
capacitor from V+ to ground is applicable for
single-supply applications.
- Separate grounding for analog and digital portions of circuitry is one of the
simplest and most-effective methods of noise suppression. One or more layers on
multilayer PCBs are usually devoted to ground planes. A ground plane helps distribute
heat and reduces EMI noise pickup. Make sure to physically separate digital and analog
grounds paying attention to the flow of the ground current.
- To reduce parasitic coupling, run the input
traces as far away from the supply or output
traces as possible. If these traces cannot be kept
separate, crossing the sensitive trace
perpendicular is much better as opposed to in
parallel with the noisy trace.
- Place the external components as close to the
device as possible. As illustrated in Figure 8-8, keep RF and RG close to the inverting input to
minimize parasitic capacitance.
- Keep the length of input traces as short as
possible. Always remember that the input traces
are the most sensitive part of the circuit.
- Consider a driven, low-impedance guard ring
around the critical traces. A guard ring can
significantly reduce leakage currents from nearby
traces that are at different potentials.
- For best performance, clean the PCB following
board assembly.
- Any precision integrated circuit may experience
performance shifts due to moisture ingress into
the plastic package. Following any aqueous PCB
cleaning process, bake the PCB assembly to remove
moisture introduced into the device packaging
during the cleaning process. A low temperature,
post cleaning bake at 85°C for 30 minutes is
sufficient for most circumstances.