SBOS283D September 2003 – March 2018 REF1112
PRODUCTION DATA.
When using the REF1112 as a reference, determine the following:
To design using the REF1112, is it important to ensure that the VS is larger than VREF.
The resistor RBIAS sets the cathode current of the REF1112, IR. Ensure that this current remains in the operational region of the part for the entire VS and load range.
Using this information, select a RBIAS such that:
IREFMIN < IREF < IREFMAX where IREFMAX = 5 mA.
In this application the IREF is the operating current of the REF1112 plus the maximum possible ILOAD under no-load conditions.