SNLS698A April 2021 – September 2023 TDES960
PRODUCTION DATA
The TDES960 receiver will adapt by default based on the V3Link error checking during the Adaptive Equalization process. The specific errors linked to equalizer adaption, V3Link clock recovery error, packet encoding error, and parity error can be individually selected in AEQ_CTL register 0x42. Errors are accumulated over 1/2 of the period of the timer set by the ADAPTIVE_EQ_RELOCK_TIME. If the number of errors is greater than the programmed threshold (AEQ_ERR_THOLD), the AEQ will attempt to increase the EQ setting.