SLYS049A March 2025 – June 2025 TMAG5133
PRODUCTION DATA
The TMAG5133 X1LGA package is available with two unipolar outputs. OUT1 responds to a positive magnetic flux density through the package, which can be seen for example when a south magnet is located at the pin 1 and 4 side of the package, or when a north magnet is located at the pin 3 and 2 side of the package. OUT2 responds to a negative magnetic flux density through the package, which can be seen for example when a north magnet is located at the pin 1 and 4 side of the package, or when a south magnet is located at the pin 3 and 2 side of the package. Figure 7-4 illustrates the behavior of OUT1 and OUT2.