SLYS045A June 2021 – September 2021 TMAG5273
PRODUCTION DATA
In this mode the TMAG5273 can be configured to go to sleep and wake up at a certain interval, and measure sensor data based off the SLEEPTIME register bits setting. The device can be set to generate an interrupt through the INT_CONFIG_1 register. Once the conversion is complete and the interrupt condition is met, the TMAG5273 will exit the W&S mode and go to the stand-by mode. The last measured data will be stored in the corresponding result registers before the device goes to the stand-by mode. If the interrupt condition isn't met, the device will continue to be in the W&S mode to wake up and measure data at the specified interval. A primary can wake up the TMAG5273 anytime during the W&S mode through I2C bus or INT pin. The time it takes for the device to go to stand-by mode from W&S mode is denoted by Tstart_sleep.