SBOS820C September 2019 – June 2025 TMCS1100
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Propagation delay is the time period between the input current waveform reaching 10% of the final value and VOUT reaching 10% of the final value. This propagation delay is heavily dependent upon the alignment of the input current step and the sampling period of the TMCS1100, as shown for several different sampling window cases in Figure 7-3.
Response time is the time period between the input current reaching 90% of the final value and the output reaching 90% of the final value, for an input current step sufficient to cause a 1V transition on the output. Figure 7-3 shows the response time of the TMCS1100 under three different time cases. Unless a step input occurs directly during the beginning of one sampling window the response time includes two sampling intervals.