SBOS702D October 2014 – December 2018 TMP102-Q1
PRODUCTION DATA.
The first byte transmitted by the master is the slave address, with the R/W bit low. The TMP102-Q1 then acknowledges reception of a valid address. The next byte transmitted by the master is the pointer register. The TMP102-Q1 then acknowledges reception of the pointer register byte. The next byte or bytes are written to the register addressed by the pointer register. The TMP102-Q1 acknowledges reception of each data byte. The master can terminate data transfer by generating a START or STOP condition.