SLOS887E September 2014 – December 2018 TMP112-Q1
PRODUCTION DATA.
If the desired temperature range falls in the region of slope 3, first calculate the worst-case value from 25°C to 85°C and add it to the change in temperature multiplied by the span error of slope 3. As an example, consider the temperature range of 25°C to 125°C as shown in Equation 10:
Then perform the same calculation for the minimum case as shown in Equation 12: