The eCAP module can be used in systems where accurate timing of external events is important.
Applications for eCAP include:
- Speed measurements of rotating machinery (for example, toothed sprockets sensed through Hall sensors)
- Elapsed time measurements between position sensor pulses
- Period and duty cycle measurements of pulse train signals
- Decoding current or voltage amplitude derived from duty cycle encoded current/voltage sensors
The eCAP module includes the following features:
- 4-event time-stamp registers (each 32 bits)
- Edge-polarity selection for up to four sequenced time-stamp capture events
- Interrupt on either of the four events
- Single shot capture of up to four event timestamps
- Continuous mode capture of timestamps in a four-deep circular buffer
- Absolute time-stamp capture
- Difference (Delta) mode time-stamp capture
- All of the above resources dedicated to a single input pin
- When not used in capture mode, the eCAP module can be configured as a single-channel PWM output (APWM).
The capture functionality of the Type-2 eCAP is enhanced from the Type-0 eCAP with the following added features:
- Event filter reset bit
- Writing a 1 to ECCTL2[CTRFILTRESET] will clear the event filter, the modulo counter, and any pending interrupts flags. Resetting the bit is useful for initialization and debug.
- Modulo counter status bits
- The modulo counter (ECCTL2 [MODCTRSTS]) indicates which capture register will be loaded next. In the Type-0 eCAP, it was not possible to know current state of modulo counter.
- DMA trigger source
- eCAPxDMA is added as a DMA trigger. CEVT[1–4] can be configured as the source for eCAPxDMA.
- Input multiplexer
- ECCTL0 [INPUTSEL] selects one of 128 input signals.
- EALLOW protection
- EALLOW protection is added to critical registers. To maintain software compatibility with the Type-0 eCAP, configure DEV_CFG_REGS.ECAPTYPE to make these registers unprotected.
- ECAPxSYNCINSEL register
- The ECAPSxYNCINSEL register is added for each eCAP to select an external SYNCIN. Every eCAP can have a separate SYNCIN signal.
The eCAP inputs connect to any GPIO input through the Input X-BAR. The APWM outputs connect to GPIO pins through the Output X-BAR to OUTPUTx positions in the GPIO mux. See Section 6.5.2 and Section 6.5.3.
Figure 7-46 shows the eCAP and HRCAP block diagram.
The eCAP module is clocked by PERx.SYSCLK.
The clock enable bits (ECAPx) in the PCLKCR3 register turn off the eCAP module individually (for low-power operation). Upon reset, ECAP1ENCLK is set to low, indicating that the peripheral clock is off.
The eCAP6 and eCAP7 modules can be configured as
high-resolution capture (HRCAP) submodules. The HRCAP submodule measures the
difference, in time, between pulses asynchronously to the system clock. This
submodule is new to the eCAP Type 2 module, and features many enhancements over the
Type 0 HRCAP module.
Applications for the
HRCAP include:
- Capacitive touch
applications
- High-resolution period and
duty-cycle measurements of pulse train cycles
- Instantaneous speed
measurements
- Instantaneous frequency
measurements
- Voltage measurements across an
isolation boundary
- Distance/sonar measurement and
scanning
- Flow measurements
The HRCAP submodule includes the following features:
- Pulse-width capture in either non-high-resolution or high-resolution modes
- Absolute mode pulse-width capture
- Continuous or "one-shot" capture
- Capture on either falling or rising edge
- Continuous mode capture of pulse widths in 4-deep buffer
- Hardware calibration logic for precision high-resolution capture
- All of the resources in this list are available on any pin using the Input X-BAR.
The HRCAP submodule includes one high-resolution capture channel in addition to a calibration block. The calibration block allows the HRCAP submodule to be continually recalibrated, at a set interval, with no “down time”. Because the HRCAP submodule now uses the same hardware as its respective eCAP, if the HRCAP is used, the corresponding eCAP will be unavailable.
Each high-resolution-capable channel has the following independent key resources.
- All hardware of the respective eCAP
- High-resolution calibration logic
- Dedicated calibration interrupt