SCDS384B September 2018 – August 2025 TMUX6119
PRODUCTION DATA
The on-resistance of the TMUX6119 is the ohmic resistance across the source (SA or SB) and drain (D) pins of the device. The on-resistance varies with input voltage and supply voltage. The symbol RON is used to denote on-resistance. The measurement setup used to measure RON is shown in Figure 7-1. Voltage (V) and current (ICH) are measured using this setup, and RON is computed as shown in Equation 1:
Figure 7-1 On-Resistance Measurement Setup