SBVS264B January 2017 – September 2021 TPS3850-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The
RESET pin features a programmable reset delay time that can be adjusted from 703 µs to 3.22 seconds when using adjustable capacitor timing.
RESET is an open-drain output that should be pulled up through a 1-kΩ to 100-kΩ pullup resistor. When VDD is above VDD(min),
RESET remains high (not asserted) when the SENSE voltage is between the positive threshold (VIT+(OV)) and the negative threshold (VIT-(UV)). If SENSE falls below
VIT-(UV) or rises above VIT+(OV), then
RESET is asserted, driving the
RESET pin to a low-impedance state. When SENSE comes back into the valid window, a
RESET delay circuit is enabled that holds
RESET low for a specified reset delay period (tRST). This tRST period is determined by what is connected to the CRST pin; see Figure 8-1. When the reset delay has elapsed, the
RESET pin goes to a high-impedance state and uses a pullup resistor to hold
RESET high. The pullup resistor must be connected to the proper voltage rail to allow other devices to be connected at the correct interface voltage. To ensure proper voltage levels, give some consideration when choosing the pullup resistor values. The pullup resistor value is determined by output logic low voltage (VOL), capacitive loading, and leakage current (ID); see the Section 8.1.1 section for more information.