SLDS222C October 2019 – October 2023 TPS65313-Q1
PRODUCTION DATA
Currents through both the high-side (HS) power MOSFET and the low-side (LS) power MOSFET are continuously monitored to protect the internal power MOSFETs from damage. Current through each MOSFET is compared against two threshold levels (IHS/LS_SCG_ILIM_BUCK1 and IHS/LS_OVC_LIM_BUCK1). The former is to detect a short-circuit event and the latter is to detect an overload condition where the BUCK1 regulator is loaded with a current higher than what is specified.
If either the HS MOSFET current or the LS MOSFET current exceeds their respective overload current limits (IHS_OVC_ILIM_BUCK1 and ILS_OVC_ILIM_BUCK1) an overload event is detected and the BUCK1_OVC status bit is set in the SAFETY_BUCK1_STAT1 register; however, the regulator does not shut down. As the external inductor current continues to increase, and if either the HS MOSFET current or the LS MOSFET current exceeds their respective short-circuit current limit (IHS_SCG_ILIM_BUCK1 and ILS_SCG_ILIM_BUCK1), then the HS MOSFET is turned off immediately and the LS MOSFET is turned on, until the inductor current decreases to less than the overload threshold (ILS_OVC_ILIM_BUCK1). The BUCK1 regulator is then disabled and the BUCK1_SCG status bit is set in the SAFETY_BUCK1_STAT1 register. This double-sampling scheme allows for any overcurrent event to be detected either through a HS or LS MOSFET, especially when the BUCK1 regulator operates at a low duty cycle with a high input supply voltage. The BUCK1_SCG_OFF_EN configuration bit setting selects the device response after a short-circuit detection.
If the BUCK1_SCG_OFF_EN bit is set to 1b, the following occurs:
If the BUCK1_SCG_OFF_EN bit is set to 0b, the following occurs:
The LS MOSFET is also protected by detection circuitry for cycle-by-cycle sink-current limit. This detection circuitry protects the LS MOSFET from excessive reverse current caused by switching the PH1 or PH1A pin to PGND1 or PGND1A. If the LS sinking current exceeds the ILS_SINK_BUCK1 sink-current limit, an event is detected and the BUCK1_LS_SINK_OVC SPI status bit is set in the SAFETY_BUCK1_STAT1 register. If the event duration is longer than 20 µs (typical) the BUCK1 regulator is turned off. The inductor current continues to flow to the supply at the VIN pin through the body diode of the HS MOSFET. The BUCK1_LS_SINK_OVC_OFF_EN configuration bit setting selects the device response after the LS sink current-limit detection.
If the BUCK1_LS_SINK_OVC_OFF_EN bit is set to 1b, the following occurs:
If the BUCK1_LS_SINK_OVC_OFF_EN bit is set to 0b, the following occurs:
The LS sink current-limit event can also be detected when the regulator is enabled and when its output has not been discharged to less than the voltage level defined by the VBUCK1_RESTART_LEVEL voltage. Therefore, the LS sink current-limit event is masked when the BUCK1 regulator is enabled, until the BUCK1 output voltage (VBUCK1) exceeds its UV-threshold level.