SLVSD02D March 2015 – June 2019 TPS65982
PRODUCTION DATA.
The TPS65982 features dual I2C busses with configurable addresses. The I2C addresses are determined according to the flow depicted in Figure 64. The address is configured by reading device GPIO states at boot (refer to the I2C Pin Address Setting section for details). Once the I2C addresses are established the TPS65982 enables a limited host interface to allow for communication with the device during the boot process.